• LTC2980 VPWR Unexpected Voltage drop on input

    Hello, I have an LTC2980 Power Sequencer with the input power connected similarly to shown in Figure 30 of the LTC2977 datasheet.

    The difference is that I have a Schottky Diode between the system 5V and the LTC2980 VPWR inputs.

    I am seeing a 1V drop across…

  • LTC2980 Register (MFR_CONFIG_LTC2977) Write Error

    Hello,

    I am getting an write error whenever I try to write MFR_CONFIG_LTC2977 register .

    I want to use High resolution mode to measure the current and according to data sheet the b[9] bit should be set high (b[9] Mfr_config_adc_hires). I am using i2cget…

  • ADM1266 and LTC2980 unused DAC pins

    When all DAC pins are unused for ADM1266 and LTC2980, should we left them unconnected or connect to GND?

  • LTC2980 EEPROM At Auto Power on Control

    Dear All:

    I have finished writing all power on timing control settings to LTC2980 internal EEPROM, but every boot LTC2980 is not wotking, how can I automatically set the value of the LTC2980 EEPROM on the power to boot up? ,have any S/W document or reference…

  • RE: Is LTC2977 used for sequence beyond 8ch?

    Hello Mike,

    I've recommended LTC2980 to the customer.

    Regards,

    Hiroyuki

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032