Hi
What is the frequency of the internal oscillator when we use the internal oscillator of LTC2949 ? And can i test the wavaform on the pin of P34(CLKO) ?
The frequency is 1/1.45s when I test this pin.
Hi
What is the frequency of the internal oscillator when we use the internal oscillator of LTC2949 ? And can i test the wavaform on the pin of P34(CLKO) ?
The frequency is 1/1.45s when I test this pin.
Hello,
I have an enclosed battery pack (Li-NMC) and I need to estimate the state of charge of a (70V - 50V) battery, max and min values (63V nominal). I have found a battery monitor which is LTC2949 but it doesn't include the necessary hardware in order…
Dear Expert,
For LTC2949, Would you please help to confirm whether it can be used a 8MHz crystal as external clock input? Many thanks
Dear Expert,
For LTC2949, Would you please help to confirm whether it can be used a 8MHz crystal as external clock input? Many thanks
Hi,
I am designing a BMS and for the Battery Voltage Measurement and Current Coulomb Counter, I want to use the LTC2949, the problem is that I have not fount the VBATP-VBATM minimum and maximum voltages, nor the LTSketch codes for it.
Could you please…
Whether ltc2949 has source code to provide reference, or whether there are similar solutions to provide source code reference.
At present, PCB is designed, which is not used normally.
Used in STM32 single chip microcomputer
Or do you have any other…
Hi ADIexpert
My customer asked about the xtal spec of LTC2949 (load cap, crystal output waveform...etc)
however no related spec can be found in the datasheet.
May I know if there is any constraint on the crystal ?
thanks
Ken
As is show in datesheet:
The GUI controlling the LTC2949 demo board supports converting numbers to FLOAT24. The code section of the
LTC2949 (www.analog.com/.../ltc2949.html also provides conversion functions
written in C/C ++ for this purpose.
but I can…