• Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • RE: 请问ADIS16495-1和ADIS16505-1,如何直接连接windows 10 pc使用呢。

    我们有相应的开发板和Windows版软件,在对应芯片下面都可以找到

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • HMC666_using IF pin without 1:1 transformer

    Hello Team.

    1:1 transformer applied in IF pin is expensive.

    so we want to use without transformer.

    is it possible that?

    Can you support solutions?

    thanks.

    Best regards,

    Josh

  • LTM4644-1 LT POWER CAD 3+1 MODEL,

    CAN YOU POINT ME TO THE POWER CAD MODEL FOR 3+1, I ALREADY HAVE THE 2+2 AND 4.

    I WANT TO MAKE SURE I GET THE COMPENSATION VALUES CORRECT BEFORE BUILD.

  • Composite amplifier using ADA4637-1 and ADA4870-1

    I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…

  • ADA4627-1 and ADA4637-1 Null Inputs Connection

    Hi,

    ADA4627-1 and ADA4637-1 have NULL pins which are offset adjust pins. If I do not plan to use offset adjust what should I do with the NULL pins? Leave it floating or use 100k Ohm pull-up resistors?

    Regards,

    Ivan.

  • 2 CVBS+1 LVDS input ->1 LVDS output ?

    Dears,

    Does ADI have the solution that support 2 CVBS and 1 LVDS(5 wires) input then 1 LVDS output?

    The CVBS signal is from camera and the  LVDS is from video or navigation.

    The output LVDS will display in 800x480/1024x600 screen.

    This is the siganal…

  • Powerful Combinations are Possible when 1+1>2

    It’s a new beginning for Analog Devices and Linear Technology. Together we become the high-performance analog industry leader with an innovation engine fueled by our comprehensive portfolio of analog and mixed signal products and solutions.

    We have…

  • ADA4310-1, 4311-1 with sloped PD0, PD1

    When using 4310-1 or 4311-1, with PD0 and PD1 pins taking values between 0V and whatever is considered logic high, does the amplifier behave reasonably? By that does it behave without going unstable or draining excessive current or requiring excessive…