• LTC2942-1

    Hi.

    The Sense+ pin is connected to both Charger and Load. So,I would like to know how the LTC2942 could determine the operation mode between charge and discharge.

    Thanks.

  • Problem with LTC2942

    Good afternoon everyone from Spain,

    I'm Juan Domingo, from GTG Ingenieros.

    We have used the LTC2942 in the design of an electronic card for a portable device. We have connected this IC as indicated in the datasheet. Schematic in pdf file is attached…

  • LTC2942 minimum voltage for coulomb counter

    I am currently working on a design that uses a LTC2942 with an external sense resistor of 10 mOhms and battery pack with a large capacity (13200mAH @ 4.0V).
    The LTC2942 is configured to use a prescaler of 64.

    Sleep mode current is approximately 900uA which…

  • LTC2942 ADC voltage conversion not correct (offset).

    Hello. We are using LTC2942 in our project.
    We found out that LTC2942 is producing results that are offset about 78mV (voltage reading through I2C is 78mV higher than it really is).
    We measure voltage using ProsKit MT-1710 meter. 

    We are using it with standard…

  • LTC2942锂电池电量计量

    使用LTC2942芯片测量锂电池里面还有多少mAh,测量不准,120mA的电流充电,使用电子负载120ma的恒流负载,测得每分钟1.1mAh。

  • Can the LTC2941 or LTC2942 be used with a 3-Cell Series NiCD?

    Hello.

    I'm looking at using the LTC2941 (or 2942) for use as a gas gauge for a 3-Cell In Series NiCD Pack for general gas gauging. The datasheet mentions it's designed for Li-Ion but the operating voltage checks out (even under my charger, a Powe…

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • 请问ADIS16495-1和ADIS16505-1,如何直接连接windows 10 pc使用呢。

    ADI工程师,

    1、我们开发的系统是运行在windows平台下的,现在需要添加IMU单元,请问这个能怎么通过USB连接PC或以太网口直接获取imu传感器的数据呢?

    2、请问你们的有相应的开发SDK吗?

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…