Hello,
I mistakenly used the LTC2941-1 instead of the LTC2941 on a board. The resistor I intended to use is 18mΩ. Is it possible to still use this chip, or will having an additional parallel resistor lower the resolution too much?
关于LTC2941的应用
Figure 7. Reading the LTC2941 Status Register (A)
要读取数据,先使用写命令,然后发寄存器值, 在发送读命令, 然后读取数据?
读命令都是这种操作么?之前看到的一些协议都是读就直接读,写就直接写?目前我这边标准库生成的
API也不支持这种读i2c 接口的方法?
目前使用的一般读区i2c的方法,读寄存器 01 02 03 04 05 ,读了2次之后,之后读取的数据都是0 ,不知道
什么情况?你们有关于操作LTC2941的实例么…
Hello.
I'm looking at using the LTC2941 (or 2942) for use as a gas gauge for a 3-Cell In Series NiCD Pack for general gas gauging. The datasheet mentions it's designed for Li-Ion but the operating voltage checks out (even under my charger, a Powe…
Hi,
We want to synchronize between the charger LTC4085 to the LTC2941, in order to make sure the LTC2941 always show the 100% level of the battery correctly and without the involvement of out uC .
In some cases, after 12 hours of charging the uC read…
ADI公司能源部门概述 ADI公司在高精度信号测量和控制方面处于业界领先地位,致力 于以极具成本竞争力的高质量IC实现可靠的计量、测量、监控 和控制。其产品广泛用于再生能源、输配电以及水、电、气计 量应用。ADI公司凭借在优化系统级信号处理性能方面的成熟经 验和种类丰富的产品,为开发人员提供精密、可靠、易于设计 的能源管理解决方案。
今天要为大家重磅推荐的是ADI最新解决方案———能源储存解决方案,点击
http://h.analog.com/CN-APM-RENEWABLE-EVff?ADICID…