• LTC2865 in Half Duplex mode

    I'd like to use the LTC2865 RS485 tranceiver since it has VL to that I can easily interface between 5V and 3.3V domains.  But I also need half duplex mode.  Is it possible to connect the 2865 in a way to acts like half duplex of the LTC2862?  Is this…

  • LTC3862-1 RS485 Network Biasing

    Hi All,

    As per LTC3862-1 datasheet (under "RS485 Network Biasing" section): 

    "The LTC2862-LTC2865 transceivers will operate correctly on biased, unbiased, or under-biased networks".

    Does this mean if we use LTC2862-1 in applications…

  • RE: [RS485] Proudct selection advice needed

    Hello HS, 

    We have a few options available with a built in level shifter than operates down to 1.8V. 

    Your design looks to be full-duplex so I would recommend one of the following

    • ADM3064E (3.3V or 5V powered, enhanced ESD protection, for data rates up…
  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…