• LTC2862A input protection

    In the datasheet of the LTC2862A, page 24 there is schematics of a massive input protection I'll just need in our next project. I am used connecting MOV-s shunting the inputs. Now, here they seem to protect the TBUs? Can you shortly describe the idea…

  • LTC2862A-2

    Hi all,

    I am trying to communicate with two LTC2862A-2 transceiver IC's. I set te first one on Transmit mode (DE '1') and (RE '1') and the other one on receive (DE '0') and (RE '0') hard coded in the two microcontrollers attached to it. If I send data…

  • Thermal resistance θjb for LTC2862A

    Hi,

    I would like to know thermal resistance of junction to the bottom (θjb) for LTC2862A

    The above data is not available in Datasheet, We only find θja & θjc

    Data will be helpful for thermal analysis. Appreciate your assist in…

  • RE: LTC4332 - How to connect multiple remote slaves

    Hi, 

    The LTC4332 pair is designed to service up to 3 remote SPI slaves. I'm not clear if the application needs 16 (or more) physically separate devices plugging in, or if there are 16 (or more) slaves at one location and the limitation is not enough…

  • RE: LVCMOS (3.3V) to RS485/422 Converter module

    Many RS-485 or RS-422 evaluation board can be used as a module to convert from LVTTL logic to RS-422 differential signaling. 

    RS-422 is used in many protocols and so does not have a standardized connector, but the screw terminal blocks featured on the…

  • RE: power supply of ADM3078E

    Hello, 

    The ADM3078E was designed and optimized for 3.3V power supply, and has been characterized at 3.3V only.

    The device should not be operated with a 5V power supply, with 5V power the transceiver won’t conform to all datasheet specifications. Specifications…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…