• LTC2858 vs LTC2852

    Hi,

    Can LTC2852 be used in lieu of LTC2858? Will supplying 5V to LTC2852 cause any adverse effects? Both parts have the same absolute maximum electrical ratings according to the datasheet.

    I'm asking because there is a part shortage of LTC2858.

  • LTC2852

    Hello

    I am using FPGA to control on the LTC2852, The Voh of the FPGA is 2.5V and the Vih of the LTC2852 is 2V (RO,RE,DE,DI).

    The distance between the FPGA and the LTX 2852 is 2000mil, The part will work ok?

    Roi

  • LTC2852: can LTC2852 be damaged, when interchanging A,B to Y,Z in the operation?

    Hello,

    it happened in the field that the pin A,B are interchanged to Y,Z when plugging the connector. This event damaged the transceiver.

    How could this issue be solved? I though adding some diode in series to Y,Z could avoid the flow of current into…

  • LTC2852 with no Vcc and active TxD+ signal

    Hi

    What will be the behavior of the LTC2852 in case I connect to it a RS422 driver (such as MOXA) that drives a voltage (~4v) over its TxD+ output (as it sends a constant "1" as long as the PC doesn't communicate with it).

    I would like…

  • RE: Parts: LTC2852HMS#TRPBF

    Hi,

    Thanks for the query on LTC2852. We can not guarantee a low limit for the test, usually the lower temperatures procedure lower delays. From the  test results of several production lots at hot and cold, the minimum delay for receiver is around 40 nsec…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…