• LTC2756 unipolar manual span

    I want to use the LTC2756 in a fixed unipolar application with 0 - 10 V out from a 10 V reference.

    So, I understand I need to connect M-SPAN to Vdd.

    I think I want S0, S1, S2 pins to GND, correct?

    What about the reference inverting amplifier?  I hope I…

  • LTC2756 SR0, RFLAG Output Currnet

    Hi,
    My customer is considering the LTC2756.

    So I got a question.

    How much is the maximum output current value of the SR0 pin and RFLAG pin of the LTC2756?

    Is it possible to output a current of about 15mA from these pins?

    Best Regards,

    Yuya

  • RE: What is the drive current for LTC2756?It's not in the manual

    The LTC2756 is not designed to be used as a current driver.  It should be followed with an op amp which will set the current driving ability. 

  • LTC2756 LDAC-Pin versa Write-Update-Command

    Hello,

    as I am examining the command codes of the DAC, to me it is not clear, If a low level on !LDAC-Pin does the same as the update-command?
    If I send a Write-Update-Command, is it then still necessary to pull !LDAC-Pin low afterwards? Or is it unnecessary…

  • Demo Board 1792A (LTC2756) is no more recognized by DC590B

    Hi,

    I don't know if I am here in the right Blog.

    I have already successfully connected Demo Board 1792A (LTC2756) to DC590B and was running Qick Eval software.

    Unfortunately I had a short circuit / false connection somewhere and now the DC950B…

  • RE: LTC2756的驱动电流是多少?手册中找不见

    您好,请将您的问题发布在咱们的全球技术社区哦ez.analog.com/.../

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • Precision DACs Advanced

     PDF

    This Precision DACs - Advanced module aims to deepen the knowledge of readers on precision digital-to-analog converters. The topics include the different DAC types available on the market, their key parameters and specifications that addresses common…