• Can LTC2688 or DC2873A(the evaluation board for the LTC2688) support 100k Ω load?

    Can LTC2688 or DC2873A(the evaluation board for the LTC2688) support 100k Ω load? I mean, each channel.

  • LTC2688 DAC SPICE model pinout

    HI,

    The spice model for the ltc2688 has pins that aren't defined in the data sheet.   How does the spice model work?

    Namely Vdac and  NO

    Thanks

    Matt

  • Can LTC2688 support 100k Ω load

    Can LTC2688 or DC2873A(the evaluation board for the LTC2688)  support 100k Ω load? I mean, each channel.

  • LTC2688 FAQs

    Q1:  Can I use the LTC2688 with a single supply? 

    A1:  Yes, with V- connected to GND the LTC2688 can be used with a single supply.

  • LTC2688能否支持100kΩ的负载

    LTC2688(或者DC2873A)能否支持100 kΩ的负载?如果8个通道各自连一个100kΩ的负载可以吗

  • RE: LTC2686 library for Raspberry Pico or Arduino

    Hi,

    For now you can refer to the ltc2688 no-OS drivers on github. As LTC2686 and LTC2688 are of the same family, same drivers can be used to communicate with the LTC2686 with little modification in the drivers code. 

    We're in the process of releasing console…

  • RE: DC934A, DC2026

    You are very welcome!  If you need 10V check out the LTC2664 or LTC2688 or LTC2668!

  • RE: N channel low current sensing after biasing with AD5686

    Hi Stefan, 

    Reading through your intended application and control requirements, I suggest looking at the LTC2686 (8-channel) and the LTC2688 (16-channel). The key to both of these is the integrated current sense mux out for all VDAC channels.

    LTC2686 Datasheet…

  • RE: LTC2756 unipolar manual span

    Can you use a newer DAC like the LTC2668 or LTC2688?  They also have 10V ranges and are much easier to use.