• LTC2666-16 MISO output

    Hi,

    I designed a hardware with LTC2666 16bit DAC and I want to output some signals by giving the correct commands (I hope). However, When I send command, address and data word, MISO (or SDO) word doesn't match with the previous input (MOSI or SDI) word…

  • ltc2666 REF and REFCOMP

    I want to write voltages from -10 to +10volts using the internal reference,

    In my schematic i connected V+ to +12V and V- to -12V

    I Followed the data sheet and connected REF trough a  0.1uF to ground, and REFCOMP trough 0.1uF to ground (from pin functions…

  • LTC2666-12 configuration problem

    When I config the LTC2666-12, I use 0x00301000 to write code to DAC0 and update it. But there isn't any voltage output(the output is 0V). Then I use 0x00301100 to write another code to DAC0, but there isn't any voltage output(the output is 0V),…

  • LTC2666-16 reliability question

    Hi, my application would need the assurance of no major SEL (single event latch up) during operation. 

    Is it possible to provide the SEL Threshold (in terms of MeVcm2/mg)?

    If not, is it possible to advise the the wafer fab technology for our assessment? 

  • Unsuspected Phase Shift for LTC2666 DAC output

    Hi,

    I am using an LTC2666 DAC to output processed data for my application. To test the performance of the LTC2666 I conducted a simple noise/frequency response analysis. The setup of the test is the following

    The MCU is just feeding the signal through…

  • 关于LTC2666的供电问题

    关于LTC2666的供电问题

    我要设计一个多通道高速DA转换电路

    但是我的VCC供电是5V,数字供电IOVCC供电是3.3V。V+供电5V。V-供电-5V。

    问题1:

    我用SPI指令对内部的上点范围进行编程,数据表上要求将MSP0,MSP1,MSP2,这三个引脚上拉到VCC.因为数据表中VCC的供电和IOVCC供电都是5V,所以也就不存在任何问题。但是我现在数字的供电是3.3v,所以我不大清楚将MSP0,MSP1,MSP2这三个引脚接到3.3v还是5v。

    问题2:

    数据表上很清楚的写着LDAC,TGP…

  • LTC2666-16 large nonlinearity when transitioning through midpoint

    Hi everyone.

    I've got a custom baseboard with 2 LTC2666-16's connected to an FPGA. I am using the DAC's in +/-10V output mode. When the DAC's change from code 0x7fff (nominally 0 V) to 0x8000 (-1 LSB V) the output jumps by as much as 20 mV in the wrong…

  • Software control over LT2666

    I'm using an LTC2666 with a DC590B evaluation board to output a DC signal on each of the 8 channels. Ideally, I'd like to be able to programatically control the boards, so I could for instance sweep over a wide voltage range and measure some response…

  • RE: LTC2600CGN Longevity

    The LTC2666 is the newer version of the LTC2600.  I don't anticipate the LTC2600 going anywhere, but the 2666 is newer. 

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…