• LTC2508-32 SYNC pulse width time required?

    LTC2508-32 SYNC pulse width time required?

    Thank you.

  • LTC2508-32 SDOA has no output

    Hello,

           I have a problem using LTC2508-32.The chip's  22-bit no latency output has data output, but the 32-bit filter result has no output. In my design,RDLA is pulled down to GND, MCLK=1MHz, DF=256, each conversion period has a busy signal, but the…

  • RE: Design LTC2508-32 so as to perform precise voltage measurements

    Hi Shane,

    Rather than trying to shift the ADC supply voltages which may not be entirely successful, why not use a fully differential amplifier such as the ADA4945 to shift the input voltage of your signal into the range compatible with the ADC.

    (2) Never…

  • RE: LTC2508

    The In+ input (See Figure 3 of the data sheet.) goes straight into a 45pF capacitor except for protection diodes that are normally reverse biased. The only way to draw any significant current into the input is to take the input voltage above REF or below…

  • LTC2508 - Large Ripple during large signal settling transient

    Hi

    According to the pictures in the datasheet, the LTC2508 has up to 500uV pp of noise during large signal settling. Is this really correct?

    If yes, where is this noise coming from? Does it disappear after the transient? What's the frequency range?…

  • Can ADG732 be used as both 1:32 and 32:1 configurations

    Hi ,

    silly qn. but can ADG732 be used in both mux and demux configs? bcos I saw that the description says 32 inputs to one output.. hence the qn...

  • Output code format of LTC2500-32's 32-bit no latency composite code mode

    Hello

    Now I want to use LTC2500-32 and LTC6363 to sample AC signal.And I use 32-bit no latency composite code mode which a 24-bit code representing the differential input voltage.I want to know which is the sign bit in the output data.In my code, the MCU…

  • 2011-01-07 17:32:32     incorrect image information for uImage-BF526-EZBRD-2010R1-RC5?

    2011-01-07 17:32:32     incorrect image information for uImage-BF526-EZBRD-2010R1-RC5?

    Matt Prewett (UNITED STATES)

    Message: 97263   

    I downloaded uImage-BF526-EZBRD-2010R1-RC5 from your website today. When I load this in u-boot and get the info it seems…

  • BOOTFLASH:SPI:AT45DB321D-SU 32 MB,so please tel me 32 mb will be support for ADSP-BF525

    Hi,

       We are using the ADSP-BF525,We already have SPI :AT45DB161D 16 mb  bootflash source code it is working .Now we are plannig to use SPI:AT45DB321D-SU 32 MB,so please tel me 32 mb will be support for ADSP-BF525, if it support please send me the any…

  • ADAU1701 ADC值的范围是0到2的32次方吗?假如是32位的ADC