• LTC2484 Query

    Hi Team,

    I am using LTC2484 ADC for self diagnosis purpose.

    On our custom board we have AD5420 and AD5421 DAC.

    We need LTC2484 to monitor the currents from these DAC's.

    Can I know whether I can connect like as shown in the attached figure.

    Also let…

  • LTC2484 easy drive problem

    Dear

    here is my circuit and adc output.

    I expected LTC2484 easy drive cancel the input current which caused offset and noise.

    what is the cause of this offset and noise?

    how to utilize easy driver to cancel the offset and noise?

    when I changed R20,R21…

  • LTC2484 External Caps

    LTC2484 datasheet figures 15 through 18 suggest large CREF decoupling capacitors cause gain error.  I am puzzled by this.  I would expect the opposite.  The second paragraph on page 28 is confusing.  The first sentence almost seems to suggest that the external…

  • RE: LTC2400 series ADC devices

    The LTC2400 is listed as Production on the web site. This means it is appropriate for new designs but there are newer alternatives available.

    The LTC2484 has a faster sample rate, differential inputs for better noise rejection, lower power consumption…

  • RE: AD5421 Power On Reset

    Hi Anush,

    Considering the maximum supply current drawn from the DVDD of AD5421.

    • LTC2484 = 250uA
    • ADUM1441 = 900uA (x4)
    • AD5420 = 1mA
    • AD5421 IOVDD = 300uA

    These would already be equal to 5.15mA. We haven't even added the current drawn from the pull-up…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…