• LTC2451 doesn't release SDA bus line after issuing an ACK

    Hi folks,

    it seems LTC2451 doesn't follow the normal I2C bus protocol, it holds SDA line down after issuing an ACK to master, this causes a bus collision error occurs and disrupts the transmission. the SDA line should be released after 9th clock cyc…

  • LTC6811 communication through I2C

    Hello all:

    We are trying to interface between LTC6811  and LTC2451 ADC  through I2C on gpio4 and gpio5 of 6811 module. The LTC2451 ADC will act as a temperature sensor so we can measure temperature for our battery modules. In LTC2451 data sheet, the ADC will…

  • Question about ADC Product

    Hi,

    I'm looking for a ADC IC covering the following spec.

    - Single-end 2ch input, 16bit, More than 50Hz ODR, I2C interface, Lead frame package like SOT, MSOP and TSSOP.

    But I can not find a suitable solution then I consider to use 1ch ADC x 2 parallel…

  • Simple I2C Transaction on the LTC6811

    Hi all,

    My team and I are trying to implement I2C communication between the LTC2451 (ADC) and the LTC6811(Stack Monitor). Our test setup includes a Linduino One, DC2259A, and DC1383A-A.

    Our first goal in mind is to capture any traces of I2C being written…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…