• LTC2444, LTC2448 analog input pin connection

    Hello,

    I'm DFAE. I receuved a question from my customer.

    He would like to use LTC2444 or LTC2448 for same PCB and software because of availability issue of them. He use only CH0 channel by single -ended mode. Can we short(connevt) pin 8 and pin 9 of…

  • ltc2448 input impedance problem

    Hello all,

    we're using the ltc2448 for our design (see schematic). We're able to control the ADC over SPI and we're also able to receive converted values. These values are somehow plausible.

    But during conversion time we're seeing a voltage…

  • Questions about the replacement of LTC2444

    Hi,

    I have already started mass production with LTC2444, but due to the difficulty in availability, I'm considering a running change

    to LTC2448 or LTC2445. Then I have two questions.

    1: I will not use the analog input pins (8,9,11,12,15,16,19,20,23…

  • RE: Ltc2439-1 in SPI communication data output is high first out or low first out?

    I suggested the LTC2448 not the LTC2488. The LTC2448 can have a conversion time as fast as 1.13ms. 

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…