• LTC2433 SDO Output Levels too low

    I've configured the LTC2433 in External Serial Clock, CS = 0 Operation (2-Wire) mode.

    When I actually probe the output I see the following behavior: (Yellow = SCK, Red = SDO):

    Notably, the data bits are only rising to a level of approximately 350mV…

  • RE: wants to confirm whether LT8708-1 (LT8708EUHG-1#PBF) can work independently.

    Hello,

    sometimes page one of the datasheet contains the answer:

    The LT8708-1 always operates as a slave to the master LT8708 and has the capability of delivering as much cur-rent or power as the master.

    Hence I would state, that LT8708-1 can NOT work…

  • LTM4644-1 LT POWER CAD 3+1 MODEL,

    CAN YOU POINT ME TO THE POWER CAD MODEL FOR 3+1, I ALREADY HAVE THE 2+2 AND 4.

    I WANT TO MAKE SURE I GET THE COMPENSATION VALUES CORRECT BEFORE BUILD.

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • HMC666_using IF pin without 1:1 transformer

    Hello Team.

    1:1 transformer applied in IF pin is expensive.

    so we want to use without transformer.

    is it possible that?

    Can you support solutions?

    thanks.

    Best regards,

    Josh

  • RE: adum4121-1 voltage

    Hi Mehdi,

    which voltage exactly do you mean?

    Vdd1 can have 5V, and min input voltage (VIH) for signal inputs can be >0.7 x Vdd1. 

  • Composite amplifier using ADA4637-1 and ADA4870-1

    I want to build a composite amplifier using the Figure 77 of the datasheet ADA4870-1. It says that the voltage offset is less than 500 uV. I simulate this circuit using LTSpice, when driving ada4637-1 with 0V and monitor the output of ADA4870-1, it is…