• CNVST pin of LTC2389-16

    Hi, 

    I would like to ask a question about  CNVST pin on LTC2389.

    The datasheet says the pin CNVST's logic level is determined by VDD, not OVDD. But the demo schematic on page 37 shows the CNVST is drived by a 3.3V signal, means its logic level is determined…

  • Common mode input voltage question about AD7622 and LTC2389-16

    I have a signal with 2.6Vpp and centered around 1.3V(VCM) and a DC voltage 1.3V(VCM).

    Now, I want to fetch these two source into LTC2389-16 or  AD7622  to have a differential bipolar AD conversion and remove common mode noise.

    And I have some question abo…

  • LTC2389

    Hi, 

    I would like to ask the range for reference voltage on LTC2389. Let say I want the input range to be 3V. Therefore, can I put 3V on the REFIN pin? 

    Thank you. 

  • 16 in 16 out DSP, Arduino

    Hi hi

    I'm starting a new project with the following specs

    1 - 16 analog audio inputs 
    2 - 16 analog audio outputs 
    4 - Matrix mixing capability 
    5 - Uses SigmaStudio 
    6 - Minimum sample rate = 96 KHz

    Which DSP chip would you recommend?

    Is ADAU144x my best…

  • 11/16/16 The Art of Military Communications

    11/16/16 The Art of Military Communications
  • Internal Reference characteristics - LTC2326-16

    Hi,

    We were looking at the Internal Reference (REFIN) characteristics in page 4 of the data sheet of LTC2326-16. We see that the temperature Coefficient for the voltage at REFIN mentioned in the table is Typical : 2 ppm/°C and Maximum : 20 ppm/°C…

  • 16 Input / 16 Output Mixer with AD1939 + AD1974

    Hi there,

    I am designing a digital audio mixer with 16 audio input channels and 16 output channels. A combined DSP/ARM provides processing and Ethernet capabilities.

    In order to speed up the process, I'm using a module that includes an OMAPL138. In…

  • 11/16/16 The Art of Military Communications

    This webcast gives an overview of recent trends in radio hardware in the military communications (MILCOM) field including what technologies and requirements are driving these trends. The main focus will be the shift to more widespread satellite communications…

  • 2010-03-16 10:16:23     Is Asterisk ported ?

    2010-03-16 10:16:23     Is Asterisk ported ?

    Emil Bart (POLAND)

    Message: 87261   

    Hello all,

    I would like to ask if asterisk app in user directory have been ported to uClinux distribution (release 2009R1.1-RC4)? Can I enable it in user config and compile…

  • 2010-12-16 16:06:32     Automated autoconf.h generation.

    2010-12-16 16:06:32     Automated autoconf.h generation.

    Matt Gilg (UNITED STATES)

    Message: 96816   

    I'm assembling scripts to automatically pull in our vendor modifications & configuration and build the distribution.

    Currently, I copy our vendor…