• 2009-12-18 09:50:18     upgrading

    2009-12-18 09:50:18     upgrading

    Filip Vanalme (BELGIUM)

    Message: 83699   

    Hi,

    I'm finally upgrading to the latest versions of toolchain and kernel. I installed blackfin-toolchain-09r1-10.i386.rpm and blackfin-toolchain-uclibc-default-09r1-10.i386.rpm…

  • 2008-02-18 04:18:22     struct video_device

    2008-02-18 04:18:22     struct video_device

    stop go (UNITED STATES)

    Message: 51190    Hi,

    I'm trying to compile the kernel, and my compile is breaking due to what appears to be some sort of video driver framework disjoint.

    /include/media/v4l2-dev.h…

  • LTC2326-18 Behavior if reading less than 18 bits

    Can anyone tell me the behavior of the LTC2326-18 if you only clock out 16 bits between conversions.  We thought we would simply get the most significant 16 bits and the bottom 2 bits would be discarded when the next conversion is started, however, we are…

  • 2010-11-18 08:12:18     Alsa driver issue

    2010-11-18 08:12:18     Alsa driver issue

    Shyam sundar (INDIA)

    Message: 95944   

    Hello world,

    I am using Alsa 1.0.18 on BF537 board.

    When I try to list the sound cards on the board,I do get the following message

    root:/> aplay -l

    **** List of PLAYBACK…

  • 2008-11-18 18:16:54     Run in ADSP-BF535??

    2008-11-18 18:16:54     Run in ADSP-BF535??

    Antonio Carmona (SPAIN)

    Message: 65461   

    Hello,

    I'm new to the forum and again in the development of embedded systems, I chose the Blackfin to venture into this passionate world. I have the opportunity to get…

  • AD7606C-18

    So, im using the ad7606c-18 instead of the -16, and I use a SCLK with 16.67 MHz and works correctly, but when I increase it to 25 MHz it does not work. I'm using the EVAL-AD7606C18FMCZ board.

    Another question that I have, if you know if the FlexSPI…

  • 2006-05-25 18:18:32     ppifcd_test on BF537-STAMP

    2006-05-25 18:18:32     ppifcd_test on BF537-STAMP

    Michael Benjamin (UNITED STATES)

    Message: 7963    Does the ppifcd_test Blackfin-Test program work on the BF537-STAMP board? If so, could someone help me?

    I currently have the following Kernel settings:

  • 2010-03-22 18:18:04     pata_pcmcia CompactFLASH load error

    2010-03-22 18:18:04     pata_pcmcia CompactFLASH load error

    Doug Bailey (UNITED STATES)

    Message: 87593   

    I am running the 2009R1.1-RC4 tag distro on a BF537 based board.  Configured on

    this board is a pcmcia slot used for interfacing a compactflash drive…

  • 2009-07-18 11:18:11     PORTMUX and PORTFER Configuration doubt

    2009-07-18 11:18:11     PORTMUX and PORTFER Configuration doubt

    Appalayagari Sreedhar (INDIA)

    Message: 77608   

    Hi,

    I am working with 2009R1-RC1 distribution with BF527 based custom hardware.

    I need to configure the PORTMUX and PORTFER registers according…

  • 2009-08-21 10:18:18     ppi_test can't open /dev/ppi

    2009-08-21 10:18:18     ppi_test can't open /dev/ppi

    xm ye (CHINA)

    Message: 79121   

    hi ,

    i used ppi driver , when sytem started,it have the node   /dev/ppi,and in /proc/misc also have info  "249 ppi",  but when  i use ppitest it can't open the…