• parameter in LTC2378-20

    Hello everyone,

    I just need a very fast confirm from someone of you. I am looking at the datasheet of the LTC2378-20

    At pag 3 in the "dynamic accuracy section", there is a parameter  called A_IN.

    what is that parameter?

    My guess is that is…

  • LTC2378-20: Behaviour of DGC Pin

    Hello

    The reference designs of LTC2378-20, DC1925A and DC2135A both have a 100nF capacitor close to the REF/DGC input (pin 7).

    We do not use DGC, so we tie this input to the reference voltage.
    Can we connect it directly to the REF input on pin 8, omitting…

  • How does the LTC2378-20 behave when over driven?

    Is the output code limited to minimum or maximum? Or does the code "roll over"?

  • Questions about the LPF of input signal chain of LTC2378-20

    Dear Analog Engineer Zone, 

    While I was looking at LTC2378-20 ADC, I have a question regarding the RC network as shown in the attachment, which is on P10 of the datasheet. 

    -- How did you define LPF1 resistor and capacitor value and how did you define the…

  • 16 in 16 out DSP, Arduino

    FormerMember
    FormerMember

    Hi hi

    I'm starting a new project with the following specs

    1 - 16 analog audio inputs 
    2 - 16 analog audio outputs 
    4 - Matrix mixing capability 
    5 - Uses SigmaStudio 
    6 - Minimum sample rate = 96 KHz

    Which DSP chip would you recommend?

    Is ADAU144x my best…

  • 11/16/16 The Art of Military Communications

    11/16/16 The Art of Military Communications
  • AD7606C-16 Digital Interface

    Hi Team,

    Does AD7606C-16 supports standard SPI interface for digital data interface?

    Thanks

    Anand B

  • 16 Input / 16 Output Mixer with AD1939 + AD1974

    Hi there,

    I am designing a digital audio mixer with 16 audio input channels and 16 output channels. A combined DSP/ARM provides processing and Ethernet capabilities.

    In order to speed up the process, I'm using a module that includes an OMAPL138. In…

  • 11/16/16 The Art of Military Communications

    This webcast gives an overview of recent trends in radio hardware in the military communications (MILCOM) field including what technologies and requirements are driving these trends. The main focus will be the shift to more widespread satellite communications…

  • 2010-03-16 10:16:23     Is Asterisk ported ?

    2010-03-16 10:16:23     Is Asterisk ported ?

    Emil Bart (POLAND)

    Message: 87261   

    Hello all,

    I would like to ask if asterisk app in user directory have been ported to uClinux distribution (release 2009R1.1-RC4)? Can I enable it in user config and compile…