• LTC2376-16

    Difference between DC1805A-D and DC1783A-D

  • LTC2376-20 clock speed

    Hi

    I need help with LTC2376-20 (and family). In my application I don't need to sample more than 1ksps to 10ksps, my question is what is the lowest clock (SCK) I can run LTC2376-20 SPI interface at? Can I supply a 5 or 10Mhz clock? I am planning to interface…

  • RE: Difference between AD7606C-16 and LTC2358-16

    Thanks for reply and sorry for my late response. There is a Vx- absolute voltage table in datasheet, and according to this table, this room looks very tight. When I sense the differential signal, how can I calculate the absolute voltage of Vx-? Because…

  • 16 in 16 out DSP, Arduino

    FormerMember
    FormerMember

    Hi hi

    I'm starting a new project with the following specs

    1 - 16 analog audio inputs 
    2 - 16 analog audio outputs 
    4 - Matrix mixing capability 
    5 - Uses SigmaStudio 
    6 - Minimum sample rate = 96 KHz

    Which DSP chip would you recommend?

    Is ADAU144x my best…

  • 11/16/16 The Art of Military Communications

    11/16/16 The Art of Military Communications
  • 16 Input / 16 Output Mixer with AD1939 + AD1974

    Hi there,

    I am designing a digital audio mixer with 16 audio input channels and 16 output channels. A combined DSP/ARM provides processing and Ethernet capabilities.

    In order to speed up the process, I'm using a module that includes an OMAPL138. In…

  • 11/16/16 The Art of Military Communications

    This webcast gives an overview of recent trends in radio hardware in the military communications (MILCOM) field including what technologies and requirements are driving these trends. The main focus will be the shift to more widespread satellite communications…

  • 2010-03-16 10:16:23     Is Asterisk ported ?

    2010-03-16 10:16:23     Is Asterisk ported ?

    Emil Bart (POLAND)

    Message: 87261   

    Hello all,

    I would like to ask if asterisk app in user directory have been ported to uClinux distribution (release 2009R1.1-RC4)? Can I enable it in user config and compile…

  • 2010-12-16 16:06:32     Automated autoconf.h generation.

    2010-12-16 16:06:32     Automated autoconf.h generation.

    Matt Gilg (UNITED STATES)

    Message: 96816   

    I'm assembling scripts to automatically pull in our vendor modifications & configuration and build the distribution.

    Currently, I copy our vendor…

  • 2009-03-09 16:16:14     Mounting jffs2 partition

    2009-03-09 16:16:14     Mounting jffs2 partition

    Steven Vacca (UNITED STATES)

    Message: 70622   

    I am having troble getting my jffs2 partition mounted.

    My Environment:   bf537 dev unit, m25p128 FLASH

    --------------------------------------

    Kernel boot-up…