I want to use LTC2373-16 for high speed data acquisition.
I have purchased evaluation board DC2071 and the compatible interface card Linduino 2026C.
Quickeval and LTC2374.exe (there is no link provided for LTC2373) do not have options for acquiring data…
Hi,As I did not get any answer to my question from CIC EMEA so far , I will try this way...
I use the LTC2373-16 ADC. In the datasheet it is written that the REFIN pin should be decoupled with a 100nF ceramic capacitor. But in the Eval Board schematic…
2009-12-18 09:50:18 upgrading
Filip Vanalme (BELGIUM)
Message: 83699
Hi,
I'm finally upgrading to the latest versions of toolchain and kernel. I installed blackfin-toolchain-09r1-10.i386.rpm and blackfin-toolchain-uclibc-default-09r1-10.i386.rpm…
There is no IBIS model available for the LTC2338. The LTC2380 is a very similar product which does have an IBIS model.
2008-02-18 04:18:22 struct video_device
stop go (UNITED STATES)
Message: 51190 Hi,
I'm trying to compile the kernel, and my compile is breaking due to what appears to be some sort of video driver framework disjoint.
/include/media/v4l2-dev.h…
2010-11-18 08:12:18 Alsa driver issue
Shyam sundar (INDIA)
Message: 95944
Hello world,
I am using Alsa 1.0.18 on BF537 board.
When I try to list the sound cards on the board,I do get the following message
root:/> aplay -l
**** List of PLAYBACK…
2008-11-18 18:16:54 Run in ADSP-BF535??
Antonio Carmona (SPAIN)
Message: 65461
Hello,
I'm new to the forum and again in the development of embedded systems, I chose the Blackfin to venture into this passionate world. I have the opportunity to get…
2006-05-25 18:18:32 ppifcd_test on BF537-STAMP
Michael Benjamin (UNITED STATES)
Message: 7963 Does the ppifcd_test Blackfin-Test program work on the BF537-STAMP board? If so, could someone help me?
I currently have the following Kernel settings:
2010-03-22 18:18:04 pata_pcmcia CompactFLASH load error
Doug Bailey (UNITED STATES)
Message: 87593
I am running the 2009R1.1-RC4 tag distro on a BF537 based board. Configured on
this board is a pcmcia slot used for interfacing a compactflash drive…
2009-07-18 11:18:11 PORTMUX and PORTFER Configuration doubt
Appalayagari Sreedhar (INDIA)
Message: 77608
I am working with 2009R1-RC1 distribution with BF527 based custom hardware.
I need to configure the PORTMUX and PORTFER registers according…