Hi,As I did not get any answer to my question from CIC EMEA so far , I will try this way...
I use the LTC2373-16 ADC. In the datasheet it is written that the REFIN pin should be decoupled with a 100nF ceramic capacitor. But in the Eval Board schematic…
I want to use LTC2373-16 for high speed data acquisition.
I have purchased evaluation board DC2071 and the compatible interface card Linduino 2026C.
Quickeval and LTC2374.exe (there is no link provided for LTC2373) do not have options for acquiring data…
Hi hi
I'm starting a new project with the following specs
1 - 16 analog audio inputs 2 - 16 analog audio outputs 4 - Matrix mixing capability 5 - Uses SigmaStudio 6 - Minimum sample rate = 96 KHz
Which DSP chip would you recommend?
Is ADAU144x my best…
Sorry for the late revert. Just resumed the project activity. The digital host is Zynq 7020 SoC.
Have provisioned for 2 ADCs in the PCB for the 16 single ended unipolar analog inputs. With respect to the data output, SPI will be the data interface to the…
Hi there,
I am designing a digital audio mixer with 16 audio input channels and 16 output channels. A combined DSP/ARM provides processing and Ethernet capabilities.
In order to speed up the process, I'm using a module that includes an OMAPL138. In…
This webcast gives an overview of recent trends in radio hardware in the military communications (MILCOM) field including what technologies and requirements are driving these trends. The main focus will be the shift to more widespread satellite communications…
2010-03-16 10:16:23 Is Asterisk ported ?
Emil Bart (POLAND)
Message: 87261
Hello all,
I would like to ask if asterisk app in user directory have been ported to uClinux distribution (release 2009R1.1-RC4)? Can I enable it in user config and compile…
2010-12-16 16:06:32 Automated autoconf.h generation.
Matt Gilg (UNITED STATES)
Message: 96816
I'm assembling scripts to automatically pull in our vendor modifications & configuration and build the distribution.
Currently, I copy our vendor…
1. The CLK frequency can go up to 400MHz. There is no minimum CLK frequency
2. ENOB= (SINAD -1.76)/6.02 = (93.9-1.76)/6.02 = 15.3Bits for a 2kHz input signal at 10Msps