• 2009-02-09 18:10:18     bug in i2c-bfin-twi.c?

    2009-02-09 18:10:18     bug in i2c-bfin-twi.c?

    Frank Shew (UNITED STATES)

    Message: 69152   

    We have a custom BF537 board with an I2C RTC (MAX DS3231) running uclinux 2007R1 for some time.  Recently during migration to 2008R1.5-RC3 we losted access to the…

  • 2010-03-18 01:18:15     trouble getting started with BF537-STAMP

    2010-03-18 01:18:15     trouble getting started with BF537-STAMP

    Hugh Shane (UNITED STATES)

    Message: 87362   

    Hi,

    I'm having trouble building a plain old bootable kernel image for the BF537-STAMP.

    U-boot: 1.1.6-svn

    toolchain: 09r1.1-2

    uClinux-dist…

  • 2011-04-08 18:51:18     [fork] "function is not implemented on no-mmu systems"

    2011-04-08 18:51:18     [fork] "function is not implemented on no-mmu systems"

    Gilles Ganault (FRANCE)

    Message: 99706   

    Hello

    I was trying to compile the opkg application and got those warning:

    ...

    LINK  opkg-cl

    ../libopkg/.libs/libopkg.so…

  • Problem reading data out of AD7606C-18

    Hi,

    I am trying to interface EVAL-AD7606CFMCZ to a Raspberry Pi Pico. I am having problem reading data out of the ADC. For a start, I tried reading the register address 0x2F which should return 0x31 for my board. But it is returning 0x00 (when CPHA is…

  • 2011-08-18 18:08:12     How i can disable GPIO request for Push Buttons(PB1 PB2 PB3 PB4 on BF548)

    2011-08-18 18:08:12     How i can disable GPIO request for Push Buttons(PB1 PB2 PB3 PB4 on BF548)

    barreh walid (TUNISIA)

    Message: 103007   

    HI

    I have a BF548 ezkit and I am using the latest trunk kernel/uboot/filesystem ( 2010R1 ).

    How i can disable…

  • RE: LTC2387-18 Shift Register Reset

    After power powering up or exiting power-down, the next two conversions produce invalid data. Subsequent conversions will produce valid data as long as the time between conversions meets the tcyc specification. There is no procedure necessary to reset…

  • LTC2358-18

    ADI/linear工程师:

    您好!近期购买了一款LTC2385-18的AD芯片,想了解一下这款芯片的最高采样率是多少?非常感谢!

  • RE: LTC2328CMS-18#PBF

    You can use the Insert tool to send files. Without the files I cannot answer your question.

  • LTC2328CMS-18#PBF

    Dear Engineering Manager

    ADILTC2328CMS-18PBF

    We need your kind advice.

    After we supplied goods, customer reported goods are NG, as attached report.

    Left side ---- OK goods

    Right side--- NG goods

    Do you think Right side is NG goods?

    We are afraid that…

  • LTC2328CMS-18#PBF

    Please send me email, i want to send attached file.

    m.ito@takumi-hkg.com

    We need your kind advice.

    After we supplied goods, customer reported goods are NG, as attached report.

    Left side ---- OK goods

    Right side--- NG goods

    Do you think Right side is…