Hi,As I did not get any answer to my question from CIC EMEA so far , I will try this way...
I use the LTC2373-16 ADC. In the datasheet it is written that the REFIN pin should be decoupled with a 100nF ceramic capacitor. But in the Eval Board schematic…
Hi John,
The LTC2324-16 data sheet is being revised. Table 2 will be changed as shown below
The doc sheet that came with the DC2395A-C states "alternatively, by connecting the DC2395A into a customer application, the performance of the LTC2325 can be evaluated directly in that circuit". How can I get more information? The docs include…
Hi,
I designed a hardware with LTC2666 16bit DAC and I want to output some signals by giving the correct commands (I hope). However, When I send command, address and data word, MISO (or SDO) word doesn't match with the previous input (MOSI or SDI) word…
We are using AD7193 in our product for Load Cell measurement. Performance of it is quiet good. Now we are in need of a similar ADC with 16-bit resolution.
16-bit, PGA, SPI, 50Hz rejection, decimate filters, filter word selection, offset correction…
Thanks Lars, that did the trick. Looks like the answer was staring me in the face. "mwipcore" was also being initialized to reg 43C00000.
Dear forum
I was looking for a ADC chip set with 16 bit or 24 bit resolution having capture buffer(FIFO) of 1024 samples and a interrupt line once capture buffer is half filled 512 samples the ADC interrupts the processor to read data from capture buffer…
Ok, I am working in 16-bit mode, and trying to ge the point I am writing the firmware to the ADV212. At the moment I have a simple loop that writes the values 0x0000 to 0x000f to the first 16 locations at address 0x00050000 in the ADV212, and then I read…