Dear EZ community,
I've ordered the 2289A-B and DC590 boards to read out the LTC2368-24 ADC with PYTHON.
To read out the LTC2368, there are code snippets for the 16bit and 18bit version with the DC890 board.
My question: can I simply adapt the code…
HI,
I am evaluating LTC2368-24 with the DC890B eval boards using LinearLab tools. Is it possible to work with more than 32768 samples ? I'm trying to make a continuous acquisition. I want to put data in txt file, but when I call multiple time the acquisition…
Hi Guys,
I'm having a problem with my ADC LTC2368-24 that every time the CNV signal goes high, some spikes were induced on the inputs. Thus when no signals present at the input, in which the ADC's output should be close to 0, the ADC converts the spike…
2009-09-24 02:14:24 mj2000 in bf561
xiyao liu (CHINA)
Message: 80330
我使用bf561内核中使用uclinux交叉编译器bfin-uclinux-gcc对mjepg2000的开源库形成的mjpeg2000可执行文件mj2_to_mj2 进行编译,出现如下错误:
root:/mj2000> ./mj2_to_mj2 -i huo.mj2 -o blue.mj2
NULL pointer access (probably…
Hi,
I work with demo circuit 2289A-B and the LTC2368-24 but i would change it to LTC2380-24, is it possible? Or may I change anything else on the demo bord ?
Kind regards
Pierre-louis
I was thinking about using the AD5449 for a project, and was wondering whether or not I could load in 12 bits of data for one of the DACs on the chip, and then another 12 bits of data for the other DAC in one single operation. The data sheet talks…
2011-08-24 12:52:24 Problem with PPI and continuous data
Lapo Pieri (ITALY)
Message: 103113
Hi Forum,
I'm a newby in bfin and dsp... I would build an application that read
a 3ch adc at 400kS/s for each channel, make some iir/fir filtering…
2009-09-24 11:12:24 Setting minimal frequency for CPU frequency scaling
Leonid Volpert (UNITED STATES)
Message: 80391
In our new product we are using BF-527 with core frequency 384MHz and sys frequency 96MHz.
By utilizing 'userspace' governor…
2008-04-24 11:54:24 USB Console - unable to open an initial console
Richard Aldrich (UNITED KINGDOM)
Message: 54876 I am using a USB to Serial adapter and trying to get the console to work over USB.
I've set console=ttyUSB0 in the boot args. It writes…
2009-06-24 23:20:24 help! where to download the "uClinux-dist-2008R1-RC8.tar.gz"
fa jin (AFGHANISTAN)
Message: 76282
Latest version is better,thanks,pls give me a website link to download
QuoteReplyEditDelete
2009-06-24 23:23:20 Re…