• 2289A-B with LTC2368-24

    Dear EZ community,

    I've ordered the 2289A-B and DC590 boards to read out the LTC2368-24 ADC with PYTHON.

    To read out the LTC2368, there are code snippets for the 16bit and 18bit version with the DC890 board.

    My question: can I simply adapt the code…

  • LTC2368-24 and DC890B : continuous acquisition

    HI,

    I am evaluating LTC2368-24 with the DC890B eval boards using LinearLab tools. Is it possible to work with more than 32768 samples ? I'm trying to make a continuous acquisition. I want to put data in txt file, but when I call multiple time the acquisition…

  • Inputs at LTC2368-24 got spikes every time CNV goes high

    Hi Guys,

    I'm having a problem with my ADC LTC2368-24 that every time the CNV signal goes high, some spikes were induced on the inputs. Thus when no signals present at the input, in which the ADC's output should be close to 0, the ADC converts the spike…

  • 2009-12-18 09:50:18     upgrading

    2009-12-18 09:50:18     upgrading

    Filip Vanalme (BELGIUM)

    Message: 83699   

    Hi,

    I'm finally upgrading to the latest versions of toolchain and kernel. I installed blackfin-toolchain-09r1-10.i386.rpm and blackfin-toolchain-uclibc-default-09r1-10.i386.rpm…

  • 2008-02-18 04:18:22     struct video_device

    2008-02-18 04:18:22     struct video_device

    stop go (UNITED STATES)

    Message: 51190    Hi,

    I'm trying to compile the kernel, and my compile is breaking due to what appears to be some sort of video driver framework disjoint.

    /include/media/v4l2-dev.h…

  • LTC2326-18 Behavior if reading less than 18 bits

    Can anyone tell me the behavior of the LTC2326-18 if you only clock out 16 bits between conversions.  We thought we would simply get the most significant 16 bits and the bottom 2 bits would be discarded when the next conversion is started, however, we are…

  • 2010-11-18 08:12:18     Alsa driver issue

    2010-11-18 08:12:18     Alsa driver issue

    Shyam sundar (INDIA)

    Message: 95944   

    Hello world,

    I am using Alsa 1.0.18 on BF537 board.

    When I try to list the sound cards on the board,I do get the following message

    root:/> aplay -l

    **** List of PLAYBACK…

  • 2008-11-18 18:16:54     Run in ADSP-BF535??

    2008-11-18 18:16:54     Run in ADSP-BF535??

    Antonio Carmona (SPAIN)

    Message: 65461   

    Hello,

    I'm new to the forum and again in the development of embedded systems, I chose the Blackfin to venture into this passionate world. I have the opportunity to get…

  • 2006-05-25 18:18:32     ppifcd_test on BF537-STAMP

    2006-05-25 18:18:32     ppifcd_test on BF537-STAMP

    Michael Benjamin (UNITED STATES)

    Message: 7963    Does the ppifcd_test Blackfin-Test program work on the BF537-STAMP board? If so, could someone help me?

    I currently have the following Kernel settings:

  • 2010-03-22 18:18:04     pata_pcmcia CompactFLASH load error

    2010-03-22 18:18:04     pata_pcmcia CompactFLASH load error

    Doug Bailey (UNITED STATES)

    Message: 87593   

    I am running the 2009R1.1-RC4 tag distro on a BF537 based board.  Configured on

    this board is a pcmcia slot used for interfacing a compactflash drive…