• 2289A-B with LTC2368-24

    Dear EZ community,

    I've ordered the 2289A-B and DC590 boards to read out the LTC2368-24 ADC with PYTHON.

    To read out the LTC2368, there are code snippets for the 16bit and 18bit version with the DC890 board.

    My question: can I simply adapt the code…

  • LTC2368-24 and DC890B : continuous acquisition

    HI,

    I am evaluating LTC2368-24 with the DC890B eval boards using LinearLab tools. Is it possible to work with more than 32768 samples ? I'm trying to make a continuous acquisition. I want to put data in txt file, but when I call multiple time the acquisition…

  • Inputs at LTC2368-24 got spikes every time CNV goes high

    Hi Guys,

    I'm having a problem with my ADC LTC2368-24 that every time the CNV signal goes high, some spikes were induced on the inputs. Thus when no signals present at the input, in which the ADC's output should be close to 0, the ADC converts the spike…

  • 16 in 16 out DSP, Arduino

    Hi hi

    I'm starting a new project with the following specs

    1 - 16 analog audio inputs 
    2 - 16 analog audio outputs 
    4 - Matrix mixing capability 
    5 - Uses SigmaStudio 
    6 - Minimum sample rate = 96 KHz

    Which DSP chip would you recommend?

    Is ADAU144x my best…

  • LTC2364-16: Driver GBW

    Hello,

    I'm trying to use the LTC2364-16, where the ADC input is driven by an op-amp buffer. It's a battery-powered application and I want to minimise power consumption, so the driver op-amp has a low GBW of only 350kHz. As I read the LTC2364-16 datasheet…

  • 11/16/16 The Art of Military Communications

    11/16/16 The Art of Military Communications
  • Internal Reference characteristics - LTC2326-16

    Hi,

    We were looking at the Internal Reference (REFIN) characteristics in page 4 of the data sheet of LTC2326-16. We see that the temperature Coefficient for the voltage at REFIN mentioned in the table is Typical : 2 ppm/°C and Maximum : 20 ppm/°C…

  • 16 Input / 16 Output Mixer with AD1939 + AD1974

    Hi there,

    I am designing a digital audio mixer with 16 audio input channels and 16 output channels. A combined DSP/ARM provides processing and Ethernet capabilities.

    In order to speed up the process, I'm using a module that includes an OMAPL138. In…

  • 11/16/16 The Art of Military Communications

    This webcast gives an overview of recent trends in radio hardware in the military communications (MILCOM) field including what technologies and requirements are driving these trends. The main focus will be the shift to more widespread satellite communications…

  • 2010-03-16 10:16:23     Is Asterisk ported ?

    2010-03-16 10:16:23     Is Asterisk ported ?

    Emil Bart (POLAND)

    Message: 87261   

    Hello all,

    I would like to ask if asterisk app in user directory have been ported to uClinux distribution (release 2009R1.1-RC4)? Can I enable it in user config and compile…