Dear EZ community,
I've ordered the 2289A-B and DC590 boards to read out the LTC2368-24 ADC with PYTHON.
To read out the LTC2368, there are code snippets for the 16bit and 18bit version with the DC890 board.
My question: can I simply adapt the code…
HI,
I am evaluating LTC2368-24 with the DC890B eval boards using LinearLab tools. Is it possible to work with more than 32768 samples ? I'm trying to make a continuous acquisition. I want to put data in txt file, but when I call multiple time the acquisition…
Hi Guys,
I'm having a problem with my ADC LTC2368-24 that every time the CNV signal goes high, some spikes were induced on the inputs. Thus when no signals present at the input, in which the ADC's output should be close to 0, the ADC converts the spike…
Hi hi
I'm starting a new project with the following specs
1 - 16 analog audio inputs 2 - 16 analog audio outputs 4 - Matrix mixing capability 5 - Uses SigmaStudio 6 - Minimum sample rate = 96 KHz
Which DSP chip would you recommend?
Is ADAU144x my best…
Sorry for the late revert. Just resumed the project activity. The digital host is Zynq 7020 SoC.
Have provisioned for 2 ADCs in the PCB for the 16 single ended unipolar analog inputs. With respect to the data output, SPI will be the data interface to the…
Hi there,
I am designing a digital audio mixer with 16 audio input channels and 16 output channels. A combined DSP/ARM provides processing and Ethernet capabilities.
In order to speed up the process, I'm using a module that includes an OMAPL138. In…
This webcast gives an overview of recent trends in radio hardware in the military communications (MILCOM) field including what technologies and requirements are driving these trends. The main focus will be the shift to more widespread satellite communications…
2010-03-16 10:16:23 Is Asterisk ported ?
Emil Bart (POLAND)
Message: 87261
Hello all,
I would like to ask if asterisk app in user directory have been ported to uClinux distribution (release 2009R1.1-RC4)? Can I enable it in user config and compile…
2010-12-16 16:06:32 Automated autoconf.h generation.
Matt Gilg (UNITED STATES)
Message: 96816
I'm assembling scripts to automatically pull in our vendor modifications & configuration and build the distribution.
Currently, I copy our vendor…