您好,我现在使用LTC2367-18这款AD芯片,我是每隔4us切换到多通道开关采集一个通道上的直流电压信号的值,大致每个通道采集1000个点,但是每个通道采集出来的点绘制成曲线是阶跃响应的形式,从零缓慢上升到正确的值,我想问问下这是因为这款AD芯片的输入信号的建立时间太长导致的吗?
您好,我现在使用LTC2367-18这款AD芯片,我是每隔4us切换到多通道开关采集一个通道上的直流电压信号的值,大致每个通道采集1000个点,但是每个通道采集出来的点绘制成曲线是阶跃响应的形式,从零缓慢上升到正确的值,我想问问下这是因为这款AD芯片的输入信号的建立时间太长导致的吗?
Hi hi
I'm starting a new project with the following specs
1 - 16 analog audio inputs
2 - 16 analog audio outputs
4 - Matrix mixing capability
5 - Uses SigmaStudio
6 - Minimum sample rate = 96 KHz
Which DSP chip would you recommend?
Is ADAU144x my best…
Hi there,
I am designing a digital audio mixer with 16 audio input channels and 16 output channels. A combined DSP/ARM provides processing and Ethernet capabilities.
In order to speed up the process, I'm using a module that includes an OMAPL138. In…
This webcast gives an overview of recent trends in radio hardware in the military communications (MILCOM) field including what technologies and requirements are driving these trends. The main focus will be the shift to more widespread satellite communications…
2010-03-16 10:16:23 Is Asterisk ported ?
Emil Bart (POLAND)
Message: 87261
Hello all,
I would like to ask if asterisk app in user directory have been ported to uClinux distribution (release 2009R1.1-RC4)? Can I enable it in user config and compile…
2010-12-16 16:06:32 Automated autoconf.h generation.
Matt Gilg (UNITED STATES)
Message: 96816
I'm assembling scripts to automatically pull in our vendor modifications & configuration and build the distribution.
Currently, I copy our vendor…
2009-03-09 16:16:14 Mounting jffs2 partition
Steven Vacca (UNITED STATES)
Message: 70622
I am having troble getting my jffs2 partition mounted.
My Environment: bf537 dev unit, m25p128 FLASH
--------------------------------------
Kernel boot-up…
I'm i the process of choosing an adc for a music project, the adc role is to read analog "control voltages" or "cv" that range between -10 and +10 volts, the data is used to set pitch of oscillators and control other parameters. First i chose the LTC2358…
I'm i the process of choosing an adc for a music project, the adc role is to read analog "control voltages" or "cv" that range between -10 and +10 volts, the data is used to set pitch of oscillators and control other parameters. First i chose the LTC2358…