• LTC2358-16

    I have a customer using the LTC2358-16. The device is able to accept different input voltage ranges, but in this case I am referring to the true bi-polar input. The device should operate between +10.24 and -10-24 on the inputs. They are only seeing +…

  • Choosing adc LTC2335-16 or LTC2358-16 for "music product"

    I'm i the process of choosing an adc for a music project, the adc role is to read analog "control voltages" or "cv" that range between -10 and +10 volts, the data is used to set pitch of oscillators and control other parameters. First i chose the LTC2358…

  • Choosing adc LTC2335-16 or LTC2358-16 for "music product"

    I'm i the process of choosing an adc for a music project, the adc role is to read analog "control voltages" or "cv" that range between -10 and +10 volts, the data is used to set pitch of oscillators and control other parameters. First i chose the LTC2358…

  • ltc2358

    Hi,

    while testing the 1st channel of ADC , a constant 0.4v drop is observed.

    I have set the softspan code of ADC channel to be 001 and gave an input of 4V and got the output of 3.6V, similarly for 3v - output of 2.6V, for 2v - output of 1.6V and for 1v…

  • RE: LTC1856 configuring and reading back differential channels

    If you need to measure a +/-20V span, may I suggest using the LTC2358-16 and the application circuit of Figure 15 on page 11 of AN167.  http://www.linear.com/docs/58894 This circuit will not work well using the LTC1856 because of its much lower input impedance…

  • LTC2358 and Arduino

    Has anyone played with interfacing an LTC2358 with an Arduino Due? Does the library for the Linduino (which matches the Uno) work with the Due?

    Thanks,

    Dan

  • LTC2358-18

    ADI/linear工程师:

    您好!近期购买了一款LTC2385-18的AD芯片,想了解一下这款芯片的最高采样率是多少?非常感谢!

  • RE: 请教AD7616是否兼容差分信号转换?

    同样关注,希望能跟凌特的LTC2358一样,支持任意波形信号差分输入。

  • RE: Use external FPGA with DC2365A

    Hi Mike,

    Yes, you can connect an external FPGA board to the DC2365A. There is no existing documentation for this but it should be a straightforward process. Tie node WRIN low. Tie node WRIN2 high (high is the default for this node). Remove R47 and R52…

  • RE: AD7606 bandwidth and any recommendation for my demand?

    Hi Jack,

    Please have a look to the Precision ADC Selector guide for a global view of the product offering within Simultaneous Sampling portfolio (page 7).

    https://www.analog.com/media/en/news-marketing-collateral/product-selection-guide/Precision-ADC…