• Use external FPGA with DC2365A

    Hello,

    I would like to interface an external FPGA (on an eval board) to the DC2365A-B LTC2357-18.  Is this possible?  Is there documentation describing how this can be done?

    Thanks!
    Mike

  • Digital power or Analog power, which one should I connect VDD of LTC2357-16 to?

    LTC2357-16 has four power pins. VCC, VEE, VDD and 0VDD. 

    VCC and VEE are for anolog power supply. And 0VDD is I/O interface power supply which should be supplied with didital power. 

    However for VDD, the datasheet writes " the 5V core power supply ". What…

  • RE: MCU Communication with medium sampling rate ADC (LTC2357-16)

    The microcontroller you selected is using a half duplex data transfer protocol on the QIO0/MOSI line. This is not compatible with how the LTC2357-16 operates.

    One possible solution is to use QIO0/MOSI for the SDI line and then use QIO1 to receive data…

  • 2009-12-18 09:50:18     upgrading

    2009-12-18 09:50:18     upgrading

    Filip Vanalme (BELGIUM)

    Message: 83699   

    Hi,

    I'm finally upgrading to the latest versions of toolchain and kernel. I installed blackfin-toolchain-09r1-10.i386.rpm and blackfin-toolchain-uclibc-default-09r1-10.i386.rpm…

  • LTC2358-18

    ADI/linear工程师:

    您好!近期购买了一款LTC2385-18的AD芯片,想了解一下这款芯片的最高采样率是多少?非常感谢!

  • HMC900LP5E compatibilty with LTC2387-18

    Hi,

    As datasheet says HMC900LP5E has 2vppd output and LTC2387 has maximum 4.096V diff-input. i want to use the whole range of LTC2387. Is there any way i Can use this low pass filter in front of this ADC (ltc2387) through which the full scale range of…

  • 2006-05-25 18:18:32     ppifcd_test on BF537-STAMP

    2006-05-25 18:18:32     ppifcd_test on BF537-STAMP

    Michael Benjamin (UNITED STATES)

    Message: 7963    Does the ppifcd_test Blackfin-Test program work on the BF537-STAMP board? If so, could someone help me?

    I currently have the following Kernel settings:

  • 2008-02-18 04:18:22     struct video_device

    2008-02-18 04:18:22     struct video_device

    stop go (UNITED STATES)

    Message: 51190    Hi,

    I'm trying to compile the kernel, and my compile is breaking due to what appears to be some sort of video driver framework disjoint.

    /include/media/v4l2-dev.h…