• RE: MCU Communication with medium sampling rate ADC (LTC2357-16)

    The microcontroller you selected is using a half duplex data transfer protocol on the QIO0/MOSI line. This is not compatible with how the LTC2357-16 operates.

    One possible solution is to use QIO0/MOSI for the SDI line and then use QIO1 to receive data…

  • RE: 关于AD7606和AD5756的问题

    AD7606模拟输入带宽有限,10v Range时为23kHz, 5v Range时为15kHz, 信号频率为10kHz时,已经衰减了大约10%. 可以考虑用LTC2357-16.

    ADI没有AD5756.

  • Digital power or Analog power, which one should I connect VDD of LTC2357-16 to?

    LTC2357-16 has four power pins. VCC, VEE, VDD and 0VDD. 

    VCC and VEE are for anolog power supply. And 0VDD is I/O interface power supply which should be supplied with didital power. 

    However for VDD, the datasheet writes " the 5V core power supply ". What…

  • Use external FPGA with DC2365A

    Hello,

    I would like to interface an external FPGA (on an eval board) to the DC2365A-B LTC2357-18.  Is this possible?  Is there documentation describing how this can be done?

    Thanks!
    Mike

  • 16 in 16 out DSP, Arduino

    Hi hi

    I'm starting a new project with the following specs

    1 - 16 analog audio inputs 
    2 - 16 analog audio outputs 
    4 - Matrix mixing capability 
    5 - Uses SigmaStudio 
    6 - Minimum sample rate = 96 KHz

    Which DSP chip would you recommend?

    Is ADAU144x my best…

  • Choosing adc LTC2335-16 or LTC2358-16 for "music product"

    I'm i the process of choosing an adc for a music project, the adc role is to read analog "control voltages" or "cv" that range between -10 and +10 volts, the data is used to set pitch of oscillators and control other parameters. First i chose the LTC2358…

  • Choosing adc LTC2335-16 or LTC2358-16 for "music product"

    I'm i the process of choosing an adc for a music project, the adc role is to read analog "control voltages" or "cv" that range between -10 and +10 volts, the data is used to set pitch of oscillators and control other parameters. First i chose the LTC2358…

  • 11/16/16 The Art of Military Communications

    11/16/16 The Art of Military Communications