• LTC2353-18 and DC2365A/DC890B eval boards: More than 32k samples

    I am evaluating the LTC2353-18 ADC with the DC2365A/DC890B eval boards using the Pscope software. The number of samples that can be recorded is 32768. Is it possible to increase the number of samples per recording beyond this limit?

    Thank you!

    Best…

  • LTC2353-16, SPI Mode Unclear From Datasheet

    I've made a technical request on this, but wanted to put this here too.

    When using the serial interface to communicate with the ADC, it seems as if the SPI write (SDI, to update softspan) requires a different mode than the output (SDO). The recommended…

  • 2009-12-18 09:50:18     upgrading

    2009-12-18 09:50:18     upgrading

    Filip Vanalme (BELGIUM)

    Message: 83699   

    Hi,

    I'm finally upgrading to the latest versions of toolchain and kernel. I installed blackfin-toolchain-09r1-10.i386.rpm and blackfin-toolchain-uclibc-default-09r1-10.i386.rpm…

  • RE: LTC2338-18 IBIS Models

    There is no IBIS model available for the LTC2338. The LTC2380 is a very similar product which does have an IBIS model.

  • 2008-02-18 04:18:22     struct video_device

    2008-02-18 04:18:22     struct video_device

    stop go (UNITED STATES)

    Message: 51190    Hi,

    I'm trying to compile the kernel, and my compile is breaking due to what appears to be some sort of video driver framework disjoint.

    /include/media/v4l2-dev.h…

  • 2010-11-18 08:12:18     Alsa driver issue

    2010-11-18 08:12:18     Alsa driver issue

    Shyam sundar (INDIA)

    Message: 95944   

    Hello world,

    I am using Alsa 1.0.18 on BF537 board.

    When I try to list the sound cards on the board,I do get the following message

    root:/> aplay -l

    **** List of PLAYBACK…

  • 2008-11-18 18:16:54     Run in ADSP-BF535??

    2008-11-18 18:16:54     Run in ADSP-BF535??

    Antonio Carmona (SPAIN)

    Message: 65461   

    Hello,

    I'm new to the forum and again in the development of embedded systems, I chose the Blackfin to venture into this passionate world. I have the opportunity to get…

  • 2006-05-25 18:18:32     ppifcd_test on BF537-STAMP

    2006-05-25 18:18:32     ppifcd_test on BF537-STAMP

    Michael Benjamin (UNITED STATES)

    Message: 7963    Does the ppifcd_test Blackfin-Test program work on the BF537-STAMP board? If so, could someone help me?

    I currently have the following Kernel settings:

  • 2010-03-22 18:18:04     pata_pcmcia CompactFLASH load error

    2010-03-22 18:18:04     pata_pcmcia CompactFLASH load error

    Doug Bailey (UNITED STATES)

    Message: 87593   

    I am running the 2009R1.1-RC4 tag distro on a BF537 based board.  Configured on

    this board is a pcmcia slot used for interfacing a compactflash drive…

  • 2009-07-18 11:18:11     PORTMUX and PORTFER Configuration doubt

    2009-07-18 11:18:11     PORTMUX and PORTFER Configuration doubt

    Appalayagari Sreedhar (INDIA)

    Message: 77608   

    Hi,

    I am working with 2009R1-RC1 distribution with BF527 based custom hardware.

    I need to configure the PORTMUX and PORTFER registers according…