• RE: DC2094A-A Evalboard

    Hi Thomas,

    I am the applications engineer for the LTC2348/DC2094.

    You can use QuikEval directly with the DC590 and DC2094. To use PScope you need the DC890 controller. With the DC890 controller you can also use LinearLab Tools and write your own data…

  • 16 in 16 out DSP, Arduino

    Hi hi

    I'm starting a new project with the following specs

    1 - 16 analog audio inputs 
    2 - 16 analog audio outputs 
    4 - Matrix mixing capability 
    5 - Uses SigmaStudio 
    6 - Minimum sample rate = 96 KHz

    Which DSP chip would you recommend?

    Is ADAU144x my best…

  • 11/16/16 The Art of Military Communications

    This webcast gives an overview of recent trends in radio hardware in the military communications (MILCOM) field including what technologies and requirements are driving these trends. The main focus will be the shift to more widespread satellite communications…

  • 11/16/16 The Art of Military Communications

    11/16/16 The Art of Military Communications
  • 16 Input / 16 Output Mixer with AD1939 + AD1974

    Hi there,

    I am designing a digital audio mixer with 16 audio input channels and 16 output channels. A combined DSP/ARM provides processing and Ethernet capabilities.

    In order to speed up the process, I'm using a module that includes an OMAPL138. In…

  • LTC2321-16

    Hi

    I have a question LTC2321-16.

    Is it okay if we can change the 220pF in front of the ADC to 10pF?

     

     

    Best Regards

    HOD

  • ltc2000-16

    Hi! I have problem iwth using ltc2000-16. SFDR = 47dBc(fout = 270MHZ, fdac=1200MHz) Rfsadj = 500Ω, Rload = 12,5Ω, LIN_DIS = 0, LIN_ GN = 75%, power is fine. What's the matter?

  • LTC2358-16

    I have a customer using the LTC2358-16. The device is able to accept different input voltage ranges, but in this case I am referring to the true bi-polar input. The device should operate between +10.24 and -10-24 on the inputs. They are only seeing +…