• Question about LTC2344-16 coversion accuracy

    Hi,

     

    Regarding LTC2344 conversion data, we can read it during the next conversion in progress but its accuracy will degrade according to the description in its data sheet page 31.

     

    - How much does the conversion accuracy degrade?

    - Does such conversion…

  • ltc2344 operation

    Please clarify this fo rme:

    I hope to have several of these units (~16) digitizing many channels (~64) simultaneously.

    I need to know if I can delay the SPI read of the result well after the result is determined, as I will need to read each unit in tu…

  • Best way to interface ADSP-SC584 with 2 LTC2344-18 ADCs

    I am using ADSP-SC584 for a project. For the project I am interfacing 2 external ADCs and 2 external DACs with processor. I believe I can interface LTC2344-18 ADC to SC584 using SPORTs, or SPI or ACM. But since I am interfacing many external components…

  • 16 in 16 out DSP, Arduino

    FormerMember
    FormerMember

    Hi hi

    I'm starting a new project with the following specs

    1 - 16 analog audio inputs 
    2 - 16 analog audio outputs 
    4 - Matrix mixing capability 
    5 - Uses SigmaStudio 
    6 - Minimum sample rate = 96 KHz

    Which DSP chip would you recommend?

    Is ADAU144x my best…

  • 11/16/16 The Art of Military Communications

    11/16/16 The Art of Military Communications
  • AD7606C-16 Digital Interface

    Hi Team,

    Does AD7606C-16 supports standard SPI interface for digital data interface?

    Thanks

    Anand B

  • 16 Input / 16 Output Mixer with AD1939 + AD1974

    Hi there,

    I am designing a digital audio mixer with 16 audio input channels and 16 output channels. A combined DSP/ARM provides processing and Ethernet capabilities.

    In order to speed up the process, I'm using a module that includes an OMAPL138. In…

  • 11/16/16 The Art of Military Communications

    This webcast gives an overview of recent trends in radio hardware in the military communications (MILCOM) field including what technologies and requirements are driving these trends. The main focus will be the shift to more widespread satellite communications…

  • 2010-03-16 10:16:23     Is Asterisk ported ?

    2010-03-16 10:16:23     Is Asterisk ported ?

    Emil Bart (POLAND)

    Message: 87261   

    Hello all,

    I would like to ask if asterisk app in user directory have been ported to uClinux distribution (release 2009R1.1-RC4)? Can I enable it in user config and compile…

  • 2010-12-16 16:06:32     Automated autoconf.h generation.

    2010-12-16 16:06:32     Automated autoconf.h generation.

    Matt Gilg (UNITED STATES)

    Message: 96816   

    I'm assembling scripts to automatically pull in our vendor modifications & configuration and build the distribution.

    Currently, I copy our vendor…