• 2009-02-09 18:10:18     bug in i2c-bfin-twi.c?

    2009-02-09 18:10:18     bug in i2c-bfin-twi.c?

    Frank Shew (UNITED STATES)

    Message: 69152   

    We have a custom BF537 board with an I2C RTC (MAX DS3231) running uclinux 2007R1 for some time.  Recently during migration to 2008R1.5-RC3 we losted access to the…

  • 2010-03-18 01:18:15     trouble getting started with BF537-STAMP

    2010-03-18 01:18:15     trouble getting started with BF537-STAMP

    Hugh Shane (UNITED STATES)

    Message: 87362   

    Hi,

    I'm having trouble building a plain old bootable kernel image for the BF537-STAMP.

    U-boot: 1.1.6-svn

    toolchain: 09r1.1-2

    uClinux-dist…

  • 2011-04-08 18:51:18     [fork] "function is not implemented on no-mmu systems"

    2011-04-08 18:51:18     [fork] "function is not implemented on no-mmu systems"

    Gilles Ganault (FRANCE)

    Message: 99706   

    Hello

    I was trying to compile the opkg application and got those warning:

    ...

    LINK  opkg-cl

    ../libopkg/.libs/libopkg.so…

  • RE: ADC LTC2387-18 SNR test condition

    Use a low jitter high quality RF generator such as HP8640B. I know it is old but that is what I use. The output is fed through a multipole low distortion LC filter. (I use TTE Q70 1MHz for this.)Then you have to convert from single ended to differential…

  • 2011-08-18 18:08:12     How i can disable GPIO request for Push Buttons(PB1 PB2 PB3 PB4 on BF548)

    2011-08-18 18:08:12     How i can disable GPIO request for Push Buttons(PB1 PB2 PB3 PB4 on BF548)

    barreh walid (TUNISIA)

    Message: 103007   

    HI

    I have a BF548 ezkit and I am using the latest trunk kernel/uboot/filesystem ( 2010R1 ).

    How i can disable…

  • AD7606C-18

    So, im using the ad7606c-18 instead of the -16, and I use a SCLK with 16.67 MHz and works correctly, but when I increase it to 25 MHz it does not work. I'm using the EVAL-AD7606C18FMCZ board.

    Another question that I have, if you know if the FlexSPI…

  • LTC2358-18

    ADI/linear工程师:

    您好!近期购买了一款LTC2385-18的AD芯片,想了解一下这款芯片的最高采样率是多少?非常感谢!

  • LTC2328CMS-18#PBF

     PDF

    我们需要您的意见建议;

    附件客户的分析报告,

    左边是OK,右边是NG,

    我们觉得客户的要求太严格,其实可能不是NG,

    请确认您的意见建议,谢谢,

    Best Regards,

    ITO Manabu

  • LTC2328CMS-18#PBF

    Please send me email, i want to send attached file.

    m.ito@takumi-hkg.com

    We need your kind advice.

    After we supplied goods, customer reported goods are NG, as attached report.

    Left side ---- OK goods

    Right side--- NG goods

    Do you think Right side is…

  • LTC2328CMS-18#PBF

    我们需要您的意见建议;

    附件客户的分析报告, PDF

    左边是OK,右边是NG,

    我们觉得客户的要求太严格,其实可能不是NG,

    请确认您的意见建议,谢谢,

     

     

    Best Regards,

    ITO Manabu

     

    夷藤 学(ITO Manabu

    Sales Executive

    Email:m.ito@takumi-hkg.com

    Tel: (+852) 2620 6262 M: (+852) 5666 3739

    達格美電子(香港)有限公司│Takumi Electronics (H.K.) Co.…