• Choosing adc LTC2335-16 or LTC2358-16 for "music product"

    I'm i the process of choosing an adc for a music project, the adc role is to read analog "control voltages" or "cv" that range between -10 and +10 volts, the data is used to set pitch of oscillators and control other parameters. First i chose the LTC2358…

  • LTC2335-16 CNV input

    Hi, I'm using a LTC2335-16 ADC in a project and I am a bit confused about what to do with the CNV input, from what I read the ADC conversation happens when the ADC gets input on the cnv pin, should I tie it to CS or maybe to the spi clock? Or just use…

  • SPI interface LTC2335-16

    Hi  there,

    I have a trouble with cmos spi communication need a detailed information to comprehensively understand.

    LCT2335-16 SCKI perios is 10ns and ı have tried to communicate with EPM570T100C5N.

    Should I creat 10ns period for SCKI or lower period?

  • LTC2335-16 ISOLATOR

    Hi,

    I need a digital isolator to isolate LTC2335-16. 

    Unfortunately I didnt understand Mbps ratio for digital isolators.

    Is 150Mbps ratio  OK?

  • Choosing adc LTC2335-16 or LTC2358-16 for "music product"

    I'm i the process of choosing an adc for a music project, the adc role is to read analog "control voltages" or "cv" that range between -10 and +10 volts, the data is used to set pitch of oscillators and control other parameters. First i chose the LTC2358…

  • RE: LTC2335-16 communication problem

    So just to narrow down my problem:
    Providing the configuration above(or unused analog inputs grounded), an unfaulty LTC2335-16 BUSY pin should respond to the first rising_edge of a square wave on CNV, right?

    Thanks again!

  • LTC2335-16 About Digital output sink current

    Hi,

    I would like to use LTC2335-16.

    So, I have a question. Please help me.

    Question:

    I want to estimate the power consumption in the IC.

    At that time, information on the current value consumed by the digital port is necessary.

    When using in CMOS mode…

  • LTC2335-16 glitchy output, thermally unstable

    I've got a board with 2 LTC233-16 chips connected to an FPGA module. I'm interfacing the chips to the FPGA module with single ended-mode. The two chips share the CNV, SCKI, and SDI lines. They have separate SDO, BUSY, CS, and SCKO lines. I don't use SCKO…

  • LTC2335 REFIN and REFBUF

    I want to read voltages from -10 to +10volts using the internal reference,

    In my schematic i connected VCC to +12V and VEE to -12V

    I Followed the data sheet and connected REFIN trough a  0.1uF to ground, and REFBUF trough 47uF to ground (from pin functions…