• RE: LTC2326-16 BUSY ISSUES

    Look at Figure 2 of the LTC2326-16 data sheet. The output of the ADC is encoded in 2's complement format. What you are seeing is normal performance.

  • ltc2326

    I can only get a range of +/-5V not +/-10V using the internal reference

  • LTC2326 Range

    I can only get a range of +/-5V not +/-10V using the internal reference for the LTC2326

  • 2009-12-18 09:50:18     upgrading

    2009-12-18 09:50:18     upgrading

    Filip Vanalme (BELGIUM)

    Message: 83699   

    Hi,

    I'm finally upgrading to the latest versions of toolchain and kernel. I installed blackfin-toolchain-09r1-10.i386.rpm and blackfin-toolchain-uclibc-default-09r1-10.i386.rpm…

  • RE: LTC2338-18 IBIS Models

    There is no IBIS model available for the LTC2338. The LTC2380 is a very similar product which does have an IBIS model.

  • 2008-02-18 04:18:22     struct video_device

    2008-02-18 04:18:22     struct video_device

    stop go (UNITED STATES)

    Message: 51190    Hi,

    I'm trying to compile the kernel, and my compile is breaking due to what appears to be some sort of video driver framework disjoint.

    /include/media/v4l2-dev.h…

  • 2010-11-18 08:12:18     Alsa driver issue

    2010-11-18 08:12:18     Alsa driver issue

    Shyam sundar (INDIA)

    Message: 95944   

    Hello world,

    I am using Alsa 1.0.18 on BF537 board.

    When I try to list the sound cards on the board,I do get the following message

    root:/> aplay -l

    **** List of PLAYBACK…

  • 2008-11-18 18:16:54     Run in ADSP-BF535??

    2008-11-18 18:16:54     Run in ADSP-BF535??

    Antonio Carmona (SPAIN)

    Message: 65461   

    Hello,

    I'm new to the forum and again in the development of embedded systems, I chose the Blackfin to venture into this passionate world. I have the opportunity to get…

  • 2006-05-25 18:18:32     ppifcd_test on BF537-STAMP

    2006-05-25 18:18:32     ppifcd_test on BF537-STAMP

    Michael Benjamin (UNITED STATES)

    Message: 7963    Does the ppifcd_test Blackfin-Test program work on the BF537-STAMP board? If so, could someone help me?

    I currently have the following Kernel settings:

  • 2010-03-22 18:18:04     pata_pcmcia CompactFLASH load error

    2010-03-22 18:18:04     pata_pcmcia CompactFLASH load error

    Doug Bailey (UNITED STATES)

    Message: 87593   

    I am running the 2009R1.1-RC4 tag distro on a BF537 based board.  Configured on

    this board is a pcmcia slot used for interfacing a compactflash drive…