Hi,
We were looking at the Internal Reference (REFIN) characteristics in page 4 of the data sheet of LTC2326-16. We see that the temperature Coefficient for the voltage at REFIN mentioned in the table is Typical : 2 ppm/°C and Maximum : 20 ppm/°C…
Hi,
We were looking at the Internal Reference (REFIN) characteristics in page 4 of the data sheet of LTC2326-16. We see that the temperature Coefficient for the voltage at REFIN mentioned in the table is Typical : 2 ppm/°C and Maximum : 20 ppm/°C…
Dear,
My LTC2326-16 only display +/-5V when reading using arduino
I tried to read many topic but i did not find any related one.
First I connect the LTC 2326 correctly with internal reference, I have measured REFIN 2.048V and REFBUF 4.096V -> correct…
Look at Figure 2 of the LTC2326-16 data sheet. The output of the ADC is encoded in 2's complement format. What you are seeing is normal performance.
I can only get a range of +/-5V not +/-10V using the internal reference for the LTC2326
Can anyone tell me the behavior of the LTC2326-18 if you only clock out 16 bits between conversions. We thought we would simply get the most significant 16 bits and the bottom 2 bits would be discarded when the next conversion is started, however, we are…
Hi hi
I'm starting a new project with the following specs
1 - 16 analog audio inputs
2 - 16 analog audio outputs
4 - Matrix mixing capability
5 - Uses SigmaStudio
6 - Minimum sample rate = 96 KHz
Which DSP chip would you recommend?
Is ADAU144x my best…
Hello,
I'm trying to use the LTC2364-16, where the ADC input is driven by an op-amp buffer. It's a battery-powered application and I want to minimise power consumption, so the driver op-amp has a low GBW of only 350kHz. As I read the LTC2364-16 datasheet…
Hi there,
I am designing a digital audio mixer with 16 audio input channels and 16 output channels. A combined DSP/ARM provides processing and Ethernet capabilities.
In order to speed up the process, I'm using a module that includes an OMAPL138. In…