Hi Gentleman,
Could you please detail LTC2323-14 TDSCKCLKOUT spec?
Why we do only have a minimum value in the datasheet? is there a spec for Maximum Values or is it related to a variable timing depending on application that cannot be measured?
Thank…
Data sheet says " A 105MHz external clock must be applied at the SCK pin to achieve 5Msps throughput. ". what should I do to use this ADC with different sampling rate , e.g. 3.125 Msps?
I drive ltc2323 at 5MSPS rate with fpga code ,and refer to the driven code which ADI offered.but there is a big porblem:the timing of signal sck and cnv signals are right and comply with the spec ,but I can't get back the adc value no matter what I d…
I am not an expert on the internals of an FPGA so I cannot give you a good answer as to what the difference would be. Also, depending on the BW of your signal and the FPGA you are using, the external flip flop may not be necessary. The best design practice…
Hello,
I'm trying to simulate the ADC-LTC2323 16bit in LTspice in order to measure THD value of this converter and compare it with the datasheet. The model of the LTC2323 is available in LTspice. I'm connecting two sine signals to the differential inputs…
你好,ADI工程师,最近选型多通道同步采样AD芯片,要求是精度12bit,采样率在5M--40M之间,现在看到 产品分类有两种:一种是LT2323-12 ,标明是同步多通道采样AD,另一类AD9637只是标明多通道,我看了AD9637的数据手册,它应该也能8通道同步采样。现在有两个疑问是:(1)LTC2323-12 和AD9637同步采样有什么差别?为什么AD9637不标明是 同步 多通道采样芯片。(2)AD9637-40,手册上标明CLK最小输入时钟是10M,如果输入5M时钟,芯片还能用吗?性能损失多少…
2011-01-10 14:14:47 workqueue
Chris Brissette (UNITED STATES)
Message: 97302
I have been hunting a random lockup, happens about once a week. Seems like it has something to do with the using the ttybf1 uart. I have been looking to where workqueue…
2011-09-14 14:43:03 user spi
Dario Bueno-Baques (MEXICO)
Message: 103388
Hi everybody:
I planning to develop an application for the bf537 stamp where is necessary to acquire some data from and ADC (16 bits simultaneous sample i.e like AD7655) make…
2008-05-14 14:34:13 Memory Protection
Henning Manteuffel (GERMANY)
Message: 55833
I connected an FPGA to the Blackfin address/data bus for accelerating arithmetic computations.
Is there a way to unprotect certain addresses in user space so that…