Hi
I have a question LTC2321-16.
Is it okay if we can change the 220pF in front of the ADC to 10pF?
Best Regards
HOD
Hi
I have a question LTC2321-16.
Is it okay if we can change the 220pF in front of the ADC to 10pF?
Best Regards
HOD
There is no long term drift data available for the internal reference. If this is required for your application, I suggest using an external reference such as the LTC6655.
2011-01-10 14:14:47 workqueue
Chris Brissette (UNITED STATES)
Message: 97302
I have been hunting a random lockup, happens about once a week. Seems like it has something to do with the using the ttybf1 uart. I have been looking to where workqueue…
2011-09-14 14:43:03 user spi
Dario Bueno-Baques (MEXICO)
Message: 103388
Hi everybody:
I planning to develop an application for the bf537 stamp where is necessary to acquire some data from and ADC (16 bits simultaneous sample i.e like AD7655) make…
2008-05-14 14:34:13 Memory Protection
Henning Manteuffel (GERMANY)
Message: 55833
I connected an FPGA to the Blackfin address/data bus for accelerating arithmetic computations.
Is there a way to unprotect certain addresses in user space so that…
2008-01-14 14:07:12 ~~Many Thanks~~
Kris Dickie (CANADA)
Message: 49562 I think it's important to give the BF-uClinux support team credit. I run a support forum for my company as well (although much less traffic), and I know how demanding it can become…
2011-03-14 14:18:22 Problem with CONFIG_DEBUG_EARLY_SERIAL
Timur Aydin (TURKEY)
Message: 98924
I was debugging an intermittent boot issue with my blackfin BF537-0.3 board. I defined the CONFIG_DEBUG_EARLY_SERIAL option in the hope of getting more…
2010-11-14 01:14:10 EZ-Kit for BF533
Jawad Riaz (PAKISTAN)
Message: 95825
Hi..
I am trying to install linux on a EZ kIt for Blackfin....I have configured the host PC with linux GCC and other repositories...I need help on how to configure the toolchain…
2008-09-26 14:14:15 uClinux 08r1.5 not compiling
ashwin b (INDIA)
Message: 62813
I am facing a problem in the last step: make
Here is the error I am getting:
cc -Werror -Wall -DHAVE_MKSTEMP -o cksum cksum.c crc.c print.c sum1.c sum2.c crc32.c
…2010-10-14 07:14:32 BF537 SPI driver problem
Shyam sundar (INDIA)
Message: 94514
Hello world,
The following is the C code I am executing from the Userspace interface!!
Here I am trying access SPI interface on a customised board having BF537. For…