• RE: LTC2314-14 this device consist how many input Chanel?

    The LTC2314-14 is only a single channel ADC. The closest to your requirements is the LTC2320-14. This is an octal 14-bit 1.5Msps ADC.

  • RE: What are the EEPROM ID values for LT Eval Boards?

    The correct string should be:

    LTC2320-16,D2374,DC2395A-A,YGG801T,CMOS,--------

    It looks like the string is corrupted. I would suggest returning the board to the place of purchase and let them know the board is nonfunctional. You should be able to exchange…

  • LTC2324 tCYC Time between Conversions Max time

    Q:

    LTC2324-12 Datasheet Page 5 Line:

    tCYC    Time between Conversions            (Note 11)  tCYC = tCNVH + tCONV + tREADOUT   min 0.5us  max 1000us

    and Page 6  Note 11:

    Note 11: Guaranteed by design, not subject to test.

    -----------------------------------------…

  • RE: ADXL1001 Daq system software

    Hi Sorry about the delay in response.  There are a couple of approaches that are typical when evaluating the wideband analog output accelerometer devices.

    Use a multi-channel input ADC which includes evalaution software.  I would recommend AD7768/1 as…

  • 2008-12-08 07:12:12     SPI and BF-561

    2008-12-08 07:12:12     SPI and BF-561

    Filip Vanalme (BELGIUM)

    Message: 66501   

    this item might already been discussed earlier. I looked into some forum discussions, but never found exactly what I'm looking for...

    I'm developing on a BF-561 board…

  • LTC2324-12

    I hope that I'm in the right place

    I have a question regarding the Linear LTC2324-12:

    I'm using the internal reference (my case is 2.048V) - can I use REFOUTx as an input for resistor division? please see the attached file configuration?

    Thank…

  • NVIC_SetPriorityGrouping(12);

    Hello,

    In ADI UART test examples we have:  

    /* NVIC initialization */

        NVIC_SetPriorityGrouping(12);

    but inside NVIC_SetPriorityGrouping() function is written:

    "

    The parameter PriorityGroup is assigned to the field SCB->AIRCR [10:8] PRIGROUP…

  • 2008-12-03 12:12:16     browsing svn source via web

    2008-12-03 12:12:16     browsing svn source via web

    Kyle Schlansker (UNITED STATES)

    Message: 66246   

    Is there a way I can view svn tree through the web?

    This page: http://docs.blackfin.uclinux.org/doku.php?id=version_control_systems&s[]=web&s[]=svn…