• LTC2271 HDL Source Code Request

    Dears

    my customer need LTC2271 HDL (VHDL,Verilog) Source Code, could you send a copy to me?

  • LTC2271直流信号采集结果直方图不一致的问题

    使用LTC2271IUKG#PBF做了一个DC电信号的采集电路,采样频率为10M,对两个通道的采集结果分别进行了直方图统计,如下:

    左边为A通道,右边为B通道;

    将A通道的信号送入B通道,然后进行采集,直方图如下:

    对B通道进行了FFT处理,没有发现明显的噪声:

    原理图设计如下:

    求助,B通道的异常是哪里有问题,该怎么解决,非常感谢。

    ADC a,b通道采集结果如下,已经转成了十进制

    a.txt

    b.txt

  • Does the LTC2271 need input clamps

    We're using the LTC2271. The analog inputs, could occasionally have voltages as high as 10 V. Under absolute maximum ratings on page 2 the datasheet says the range is -0.3V to VDD+0.2V (2.0V). But then note 3 on page 6 says:

    Note 3: When these pin…

  • ADC芯片LTC2180和LTC2271供电电源跟着采样频率变化的问题

    ADI工程师:

    您好,

        最近我们设计了一款用ARITIX-7为处理器,LTC2180(后面改为LTC2271也是同样的问题)为ADC的采集电路。发现给ADC的电压会采样频率的相同的约300mv的纹波,采样频率为12.5M时纹波频率为12.5M,采样频率为6.125M时纹波频率也为6.125M。

        开始推测是ADC采样是快速变化的电流导致电压不稳,并把原先给ADC供电的LDO(ADM7150-1.8)拆除,采用外部稳压电源供电,结果稳压电源上也出现300mv左右的纹波。该纹波严重影响了测量精度…

  • 使用ltc2271对正弦信号采样,出现问题

    ENC频率是8192KHz,对128K正弦信号采样,使用2lanse数据输出。请高手帮忙分析原因。

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…