• AD7821 with 12 Bit Resolution

    We are using AD7821 ADC (8 bit) in one biomedical instrument. But, now to improve accuracy, we need 12 Bit ADC. Since we have current stock of PCB's where AD7821 is used, is there any ADC IC which is pin to pin compatible to AD7821 with 12 Bit resolution…

  • Multiplexed 12 bit audio

    I have an application where the ADAU1701/2 would be ideal, but the lack of bit shift will be a problem, I have 2 input streams with each stream being audio packed as four 12 bit numbers (2x 12bit left and 2x 12bit right) I need to de-multiplex these and…

  • RE: AD7766 Is giving only 12 correct bits.Remaining 12 bits are noise.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • 2011-09-12 12:46:44     Questions about memory fragmentation

    2011-09-12 12:46:44     Questions about memory fragmentation

    Cameron Barfield (UNITED STATES)

    Message: 103364   

    We have a producted based on the BF537 STAMP design (running a BF536, though). Our next generation product is based on the BF527 EZKIT v2.

  • 2008-12-01 12:33:09     gptimer questions...

    2008-12-01 12:33:09     gptimer questions...

    John Doe (UNITED STATES)

    Message: 66098   

    what is the finest resolution that i can get with /dev/timer[0-7] ?

    QuoteReplyEditDelete

    2008-12-01 13:32:53     Re: gptimer questions...

    Robin Getz (UNITED STATES)

  • 2011-01-12 15:12:08     Linphone with MSX264 Pluggin or H264

    2011-01-12 15:12:08     Linphone with MSX264 Pluggin or H264

    Blair Fredericks (CANADA)

    Message: 97410   

    Hi,

    Can this H264 Linphone plugin be cross compiled and used with the Blackfin running uClinux.

    Any help would be appreiated.

    Best Regards,

    Blair…

  • 2009-12-12 02:26:10     Permission issue with directory create

    2009-12-12 02:26:10     Permission issue with directory create

    Jayakumar Ananthakrishnan (INDIA)

    Message: 83407   

    Hi,

    When I create directories on mounted pen drives with permissions other than "777" it is not set though I set dmask,fmask, umask to 0…

  • 2008-12-01 12:46:51     L1 data cache issue

    2008-12-01 12:46:51     L1 data cache issue

    Vasanth Nayak (INDIA)

    Message: 66099   

    HI,

            Iam having a issue where enabling D-cache gives a kernel panic. I am using 2008R1.5 kernel and building a multithreaded application. I have enabled I-cache and using…

  • 2010-12-12 07:34:58     adv7179 driver rgb2yuv

    2010-12-12 07:34:58     adv7179 driver rgb2yuv

    haiqing cao (CHINA)

    Message: 96651   

    I download the adv7179 driver for blackfin561-ezkit but It has a problem when I compile it.

    rgb2yuv(rgb_l1,yuv_l1,RGB_WIDTH) can not find where it is defined.

    void bfin_framebuffer_update…

  • 2008-12-08 12:04:36     "getty respawning too fast"

    2008-12-08 12:04:36     "getty respawning too fast"

    Harvey Sugar (UNITED STATES)

    Message: 66510   

    I have configured my uClinux system for login.  I am using the BF537 UART for my console and I have two issues:

    1.) When I log out, a screen of…