• Multiplexed 12 bit audio

    I have an application where the ADAU1701/2 would be ideal, but the lack of bit shift will be a problem, I have 2 input streams with each stream being audio packed as four 12 bit numbers (2x 12bit left and 2x 12bit right) I need to de-multiplex these and…

  • AD9238 (12-bit) Converter

    Hi,

       We are evaluating the AD9238 12-bit converter.  This part is available in 12-bit (AD9238) and 14-bit (AD9248).

    We purchased the AD9238 evaluation board.  The board description is in the datasheet but that description and schematic is for the AD9248…

  • RE: AD7766 Is giving only 12 correct bits.Remaining 12 bits are noise.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • 2009-12-04 12:29:52     Virtual Video Interface & vidcat

    2009-12-04 12:29:52     Virtual Video Interface & vidcat

    Owen OH (IRELAND)

    Message: 83095   

    Hello All,

    Just wondering if anybody had managed to get the video capture app (vidcat) & the vitual video device (vivi)?

    I'm getting

    root:/dev>…

  • 2009-12-12 06:18:27     Strange SDCard issue

    2009-12-12 06:18:27     Strange SDCard issue

    billy walton (UNITED KINGDOM)

    Message: 83425   

    Hi All,

    I have been trying to get a FAT16/FAT32 SDCard working with 2009R1

    I have enabled the relevent options in the kernel config, and can see the cards on…

  • 2008-12-01 12:46:51     L1 data cache issue

    2008-12-01 12:46:51     L1 data cache issue

    Vasanth Nayak (INDIA)

    Message: 66099   

    HI,

            Iam having a issue where enabling D-cache gives a kernel panic. I am using 2008R1.5 kernel and building a multithreaded application. I have enabled I-cache and using…

  • 2008-11-12 12:43:20     Double fault

    2008-11-12 12:43:20     Double fault

    Michael McTernan (UNITED KINGDOM)

    Message: 65166   

    Hi,

    I'm using BF537-0.3 on a custom board with 2008R1.5 patched to the top of SVN and we've got double faults, but only with no-MPU.  Building and running…

  • 2008-12-08 12:04:36     "getty respawning too fast"

    2008-12-08 12:04:36     "getty respawning too fast"

    Harvey Sugar (UNITED STATES)

    Message: 66510   

    I have configured my uClinux system for login.  I am using the BF537 UART for my console and I have two issues:

    1.) When I log out, a screen of…

  • 2008-12-01 12:33:09     gptimer questions...

    2008-12-01 12:33:09     gptimer questions...

    John Doe (UNITED STATES)

    Message: 66098   

    what is the finest resolution that i can get with /dev/timer[0-7] ?

    QuoteReplyEditDelete

    2008-12-01 13:32:53     Re: gptimer questions...

    Robin Getz (UNITED STATES)

  • 2008-12-01 08:00:12     uClinux firmware directory

    2008-12-01 08:00:12     uClinux firmware directory

    Ammar Asi (PAKISTAN)

    Message: 66077   

    Hi,

    I want to use wireless usb adapter tl-wn422g from tp-link on Blackfin Asterisk (IP-08). The driver for this adapter is zd1121 which is avaiable in uClinux kernel…