• 2011-06-14 08:14:33     Error in g_zero? (Gadget usb)

    2011-06-14 08:14:33     Error in g_zero? (Gadget usb)

    Morten Kvistgaard (DENMARK)

    Message: 101253   

    Hello there,

    We're trying to implement some device side usb on BF526 ezbrd. We can make the g_serial work. But the MS Windows driver for that one has…

  • 2008-09-26 14:14:15     uClinux 08r1.5 not compiling

    2008-09-26 14:14:15     uClinux 08r1.5 not compiling

    ashwin b (INDIA)

    Message: 62813   

    I am facing a problem in the last step: make

    Here is the error I am getting:

    cc -Werror -Wall -DHAVE_MKSTEMP -o cksum cksum.c crc.c print.c sum1.c sum2.c crc32.c

  • 2008-09-23 14:27:14     fw_setenv on CM-BF537?

    2008-09-23 14:27:14     fw_setenv on CM-BF537?

    Ben Burleson (UNITED STATES)

    Message: 62576   

    Has anyone had success using fw_setenv on the Bluetechnix CM-BF537E?

    I seem to have things configured at least half-correct becuase fw_printenv works fine:

  • 2011-03-14 14:18:22     Problem with CONFIG_DEBUG_EARLY_SERIAL

    2011-03-14 14:18:22     Problem with CONFIG_DEBUG_EARLY_SERIAL

    Timur Aydin (TURKEY)

    Message: 98924   

    I was debugging an intermittent boot issue with my blackfin BF537-0.3 board. I defined the CONFIG_DEBUG_EARLY_SERIAL option in the hope of getting more…

  • 2008-06-14 14:21:45     Framebuffer driver for ADV7171

    2008-06-14 14:21:45     Framebuffer driver for ADV7171

    Leslie Li (CHINA)

    Message: 57305   

    Hi all,

    I'm working on a ADV7171 framebuffer driver these days, but encountered some problems here.

    when I alter .fb_imageblit = cfb_imageblit, the kernel…

  • 2010-11-14 01:14:10     EZ-Kit for BF533

    2010-11-14 01:14:10     EZ-Kit for BF533

    Jawad Riaz (PAKISTAN)

    Message: 95825   

    Hi..

    I am trying to install linux on a EZ kIt for Blackfin....I have configured the host PC with linux GCC and other repositories...I need help on how to configure the toolchain…

  • LTC2314-14的問題

    您們好


    我想請問LTC2314-14的問題
    我照著附檔的電路圖走線
    我輸入一個Signal
    用微處理器經SPI讀取,然後讀出來的資料有問題
    想請問我這樣的電路圖設計,是否有問題?

  • HMC584 for VCO for 12Ghz to 14 Ghz.

    Can i Use HMC584 for VCO which need to work for 12Ghz to 14 Ghz. Can i use any additional circuit to overcome the drawback ( If ANy)

  • AD7732 Extended Range to ±14 Volts?

    Looking at the AD7732 datasheet (page 31 – top diagram),  It looks to me like the ±10V comes from a voltage divider on each leg (108.5K in series with 15.5K to a common 2.5V reference). Hence a 0.125 divider per leg.  If we also connect the next leg (2R…

  • NTSC encoder with 14 bit input

    I have a camera that outputs 14 bit of data plus sync. The signal in monochrome.  I need a composite NTSC output.

    What I am not sure of is how to input mono data to a color part. Do I just load into one of the R,G or B data lines? the same data into all…