• RE: The LTC2263 chip output different value under different temperatures

    The gain and offset errors are temperature  dependent.  To reduces these, have a good thermal layout and possibly a heat sink for the part.

  • ltc2263 power dissipation

    i have designed a circuit with the differential adc ltc2263,but the power dissipation is more than 500mW, but the datasheet of the ltc2263 said it costs just 100mW, i cannot find the reason, i really need someone to help me !

  • DC1532A-L (LTC2263-12) with MicroZed FMC Carrier Card

    Hello,

    I'd like to connect the DC1532A-L Evaluation Board to the MicroZed Board via the FMC Carrier Card. Has anyone experience if they are compatible? If I read the schematics of the evaluation board right, it has a FMC HPC Connector, but only the…

  • LTC2263-12 (DC1532A-L) is not working and can't program all registers via SPI

    Hello,

    I am trying to get the 12 Bit ADC on the Evaluation Board DC1532A-L (which houses the LTC2263-12) working with the Microzed Board connected via Microzed FMC Carrier Card. However,  I am reading only two or three different numbers no matter what…

  • 2011-01-10 14:14:47     workqueue

    2011-01-10 14:14:47     workqueue

    Chris Brissette (UNITED STATES)

    Message: 97302   

    I have been hunting a random lockup, happens about once a week. Seems like it has something to do with the using the ttybf1 uart.  I have been looking to where workqueue…

  • 2011-09-14 14:43:03     user spi

    2011-09-14 14:43:03     user spi

    Dario Bueno-Baques (MEXICO)

    Message: 103388   

    Hi everybody:

    I planning to develop an application for the bf537 stamp where is necessary to acquire some data from and ADC (16 bits simultaneous sample i.e like AD7655) make…

  • 2008-05-14 14:34:13     Memory Protection

    2008-05-14 14:34:13     Memory Protection

    Henning Manteuffel (GERMANY)

    Message: 55833   

    I connected an FPGA to the Blackfin address/data bus for accelerating arithmetic computations.

    Is there a way to unprotect certain addresses in user space so that…

  • 2008-01-14 14:07:12     ~~Many Thanks~~

    2008-01-14 14:07:12     ~~Many Thanks~~

    Kris Dickie (CANADA)

    Message: 49562    I think it's important to give the BF-uClinux support team credit. I run a support forum for my company as well (although much less traffic), and I know how demanding it can become…

  • 2011-03-14 14:18:22     Problem with CONFIG_DEBUG_EARLY_SERIAL

    2011-03-14 14:18:22     Problem with CONFIG_DEBUG_EARLY_SERIAL

    Timur Aydin (TURKEY)

    Message: 98924   

    I was debugging an intermittent boot issue with my blackfin BF537-0.3 board. I defined the CONFIG_DEBUG_EARLY_SERIAL option in the hope of getting more…

  • 2010-11-14 01:14:10     EZ-Kit for BF533

    2010-11-14 01:14:10     EZ-Kit for BF533

    Jawad Riaz (PAKISTAN)

    Message: 95825   

    Hi..

    I am trying to install linux on a EZ kIt for Blackfin....I have configured the host PC with linux GCC and other repositories...I need help on how to configure the toolchain…