• DC1532A-L (LTC2263-12) with MicroZed FMC Carrier Card

    Hello,

    I'd like to connect the DC1532A-L Evaluation Board to the MicroZed Board via the FMC Carrier Card. Has anyone experience if they are compatible? If I read the schematics of the evaluation board right, it has a FMC HPC Connector, but only the…

  • LTC2263-12 (DC1532A-L) is not working and can't program all registers via SPI

    Hello,

    I am trying to get the 12 Bit ADC on the Evaluation Board DC1532A-L (which houses the LTC2263-12) working with the Microzed Board connected via Microzed FMC Carrier Card. However,  I am reading only two or three different numbers no matter what…

  • RE: The LTC2263 chip output different value under different temperatures

    The gain and offset errors are temperature  dependent.  To reduces these, have a good thermal layout and possibly a heat sink for the part.

  • ltc2263 power dissipation

    i have designed a circuit with the differential adc ltc2263,but the power dissipation is more than 500mW, but the datasheet of the ltc2263 said it costs just 100mW, i cannot find the reason, i really need someone to help me !

  • 2008-12-08 07:12:12     SPI and BF-561

    2008-12-08 07:12:12     SPI and BF-561

    Filip Vanalme (BELGIUM)

    Message: 66501   

    this item might already been discussed earlier. I looked into some forum discussions, but never found exactly what I'm looking for...

    I'm developing on a BF-561 board…

  • 2008-12-03 12:12:16     browsing svn source via web

    2008-12-03 12:12:16     browsing svn source via web

    Kyle Schlansker (UNITED STATES)

    Message: 66246   

    Is there a way I can view svn tree through the web?

    This page: http://docs.blackfin.uclinux.org/doku.php?id=version_control_systems&s[]=web&s[]=svn…

  • 2008-12-01 12:33:09     gptimer questions...

    2008-12-01 12:33:09     gptimer questions...

    John Doe (UNITED STATES)

    Message: 66098   

    what is the finest resolution that i can get with /dev/timer[0-7] ?

    QuoteReplyEditDelete

    2008-12-01 13:32:53     Re: gptimer questions...

    Robin Getz (UNITED STATES)

  • 2008-11-12 12:43:20     Double fault

    2008-11-12 12:43:20     Double fault

    Michael McTernan (UNITED KINGDOM)

    Message: 65166   

    Hi,

    I'm using BF537-0.3 on a custom board with 2008R1.5 patched to the top of SVN and we've got double faults, but only with no-MPU.  Building and running…

  • 2010-12-20 04:32:12     cannot find -ldl

    2010-12-20 04:32:12     cannot find -ldl

    zhang zhihua (CHINA)

    Message: 96878   

    Hi,

        I want to use the openssl to do something,but when I make my program,it found that:

    "/home/opt/uClinux/bfin-uclinux/bin/../lib/gcc/bfin-uclinux/4.1.2/../../../../bfin…