• 2010-06-24 14:14:47     Stderr and stdout concatenation/redirection in shell scripts.

    2010-06-24 14:14:47     Stderr and stdout concatenation/redirection in shell scripts.

    Nikolay Razbegaev (RUSSIAN FEDERATION)

    Message: 90600   

    Hello.

    Which shell interpreter in uClinux distribution understand stderr and

    stdout concatenation? Default…

  • 用单片机硬件SPI读取LTC2313-14的14位数据问题

    单片机发出的一次是16个时钟,根据datasheet时序图,没有说明多发出的两个时钟LTC2313-14会输出什么。那在后两个时钟沿LTC2313-14会输出什么呢?

  • RE: LTC2000 using -16 as alternate for -14

    Yes, that should be fine.  We do not change the layout for between the -16 and -14 ICs. 

  • RE: LTC2313-14 bypass cap of Ref

    Hi Hiroyuki,

    I suspect the ADC will function with the smaller capacitor on the reference but the noise performance will be worse and the linearity may suffer as well.

  • [LTM9006-14]

    The Vcm on My Demo board DC1751 doesn't have output,is it wrong?And what the output type of FR and DCO ?LVDS?

  • 14-bit DTS

    Hi,

    I'm using the DTS 5.1 decoder on an adsp-21469 SHARC processor. When decoding an DTS stream which is in 14-bit format the decoding works just as with 16-bit but with an added high-frequency noise and distortion. I synchronize on the 0xE8001FFF (14…

  • LTC2175-14 EVM

    Hi

    The EVM for LTC2175-14 supports analog input from 5MHz onwards. I am interested in verifying LTC2175's low frequency performance. Do you have any other EVM with analog front end supporting DC and low frequencies

  • LTC2323-14 TDSCKCLKOUT

    Hi Gentleman, 

    Could you please detail LTC2323-14 TDSCKCLKOUT spec?

    Why we do only have a minimum value in the datasheet? is there a spec for Maximum Values or is it related to a variable timing depending on application that cannot be measured?

    Thank…

  • LTC2153-14 CLKOUT

    Hi,

    My customer is planning to employ LTC2153-14. Here are my customer question.

    (I don't have demoboard now. please tell me.)

    Q1)Input CLK signal to ENC PIN after power-on. We would like to know the CLKOUT PIN condition.

    What Is the default condition…

  • ADXL357 DRDY (pin 14)

    Hi,

    I just want to know how is the function of DRDY (pin 14) of ADXL357 when EXT_CLK=1 and EXT_SYNC=01.

    Is its function SYNC input or DRDY output?
    The info in table 14 is a little confusing.

    In comments it says "DRDY (active high) signals that data is…