• RE: RE: AD8302 phase measurement

    (1) 10 different frequency swap in 200us.( RF is around 200 MHz)

    (2)  please send source codes on this email id bhargenshah4551@gmail.com

    (3) can I use DC1945A(LTC2185) ADC board to acquire the output of AD8302 board?

  • how to store data from DC890B evaluation board into PC in excel format using Pscope software

    We are interested in DC1945A combo board and DC890B evaluation board which consist of LTC2185 ADC IC. DC890B is used to acquire data from the DC1945A and Pscope software is use  to collect and anlyse data from ADC but our aim is to store data into external…

  • ADI+Linear,组合参考电路推荐

    组合参考电路,对于 ADI 与 Linear 来说是一个新的开始。

    ADI+Linear将联手成为高性能模拟行业领先企业,提供由业界最齐全的模拟和混合信号产品和解决方案组合推动的创新引擎。今天版主就推荐几款 ADI+Linear 的参考电路组合,希望可以助您的设计一臂之力哦~

    无线电流检测组合

    无线电流检测电路克服了传统电流检测应用的诸多限制。让整个电路随同检测电阻的共模电压浮空,并在空中无线传输测量数据,电压限制也就无从谈起。

  • Some Problems about the ADC Module LTC2183

    Hello!

    I'm Chen Hongqiang, a student of Zhejiang University of technology. I encountered some problems when using the ADC module LTC2183 of analog company. I want to consult.

    I'm on the company website www.analog.com/.../218543f.pdf In the bottom…

  • Solved: DC1945A LVDS issue

    I have a question about the DC1945A Evaluationboard. I use the DC1945A: LTC2185 and LTC6409 COMBO BOARD to interface it with my zynq7000 FPGA. I read the Datasheets about the components in detail but there is an issue, which i can't understand so far.…

  • 关于analog公司ADC模块LTC2183的问题

    你好!
            我是浙江理工大学的学生陈洪强,在使用analog公司ADC模块LTC2183碰到一些问题,想咨询一下。
           我在公司网址www.analog.com/.../218543f.pdf的第14页,最右下角,看到这样一幅图,图片放在下面,这张图的输入信号为140MHz,采样频率为80Msps,以我个人现在的理解,这种情况下,AD采样出来信号有多个频率,分别为140-80=60MHz;80*2-140=20MHz;80*3-140=100MHz……说明采样后的频率分量有20M,60M,100M…
  • ADI最新中文资料大汇总(2017年10月)

    最新中文资料汇总来啦~

    系统解决方案、应用笔记、数据手册、技术文章、电路笔记……一站式下载!

    系统方案精选 APM

    数据手册 DATASHEET

    应用笔记 APPLICATION NOTE

    电路笔记 Circuit from the Lab (CFTL)

  • 《模拟对话》杂志第51卷第三期中文版,新鲜来袭

    ADI《模拟对话》汇聚了ADI全球工程师的先进设计思想,涵盖丰富实用的技术资料。近50年以来,它一直肩负着现实世界信号处理中电路、系统和软件技术交流平台的重任,刊登了有关最新模拟、数字和混合处理产品、应用、技术及工艺的大量优质文章。

    第51卷第3期新鲜出炉,是下载PDF文档还是索取印刷版,嫩们自己选择吧!

    纸质版请点击:http://h.analog.com/cn_analogdialogue?ADICID=SOME_CN_P1694 免费索取~

    PDF电子档请点击http://www.analog…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…